2017-06-30 6:12 AM
I'm currently working on a driver on an STM32F0 that joins the I2C bus as a slave device. Currently there is no mention in the reference manual on how to handle a Repeated Start Condition, does anyone know how to?
I am currently handling the I2C request in the AddressCallback and am able to make it work when all the frames are terminated by a Stop Condition but when I try to detect a Repeated Start using the NACK flag
(From RM: The bit is set by software, cleared by hardware when the NACK is sent, or when a STOP condition or an Address Matched is received, or when PE=0.), the ADDR flag of the I2C is never set meaning the ISR is never called again. Clock stretching is also enabled. #f0 #stm32f0 #stm32 #i2cSolved! Go to Solution.
2017-06-30 6:23 AM
Hi
Zikhali.Bongani
,I recommend you to have a look to I2C example under the STM32L4 firmware package it may help you to start :
STM32Cube_FW_L4_V1.8.0\Projects\STM32L496ZG-Nucleo\Examples\I2C\I2C_TwoBoards_RestartComIT
This example describes how to perform a single I2C data buffer transmission/reception between two boards in Interrupt mode and with a restart condition.
-Nesrine-
2017-06-30 6:23 AM
Hi
Zikhali.Bongani
,I recommend you to have a look to I2C example under the STM32L4 firmware package it may help you to start :
STM32Cube_FW_L4_V1.8.0\Projects\STM32L496ZG-Nucleo\Examples\I2C\I2C_TwoBoards_RestartComIT
This example describes how to perform a single I2C data buffer transmission/reception between two boards in Interrupt mode and with a restart condition.
-Nesrine-
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.