2020-12-07 9:58 PM
2020-12-08 12:20 AM
Could be a couple of things, most likely a Quad Mode setting or dummy cycles.
Did it read 0xFF when erased?
Normally when bringing up you should try the READ ID in the 1, 2 and 4-bit modes, and similarly the reads and writes
2020-12-08 1:10 AM
i have checked device ids for 1,4 qspi line, for 1 line im getting the correct device ids, for 4 qspi lines im getting the wrong values and for erase operation for 1 qspi lines im getting 0xFF and when i erased for 4 qspi lines im getting 0xCC instead of 0xFF.
why im getting 0xCC?
2020-12-08 4:20 AM
Sounds like your unspecified memory chip is not in Quad Mode.
2020-12-09 9:00 PM
im using IS25LP128/064
2020-12-10 5:50 AM
Have you tried the data sheet? http://www.issi.com/WW/pdf/IS25LP128.pdf
2020-12-14 2:24 AM
i have enabled the quad mode i.e, quad enable bit but im getting the same problem.
2020-12-14 6:10 AM
You'd be looking at several hundred dollars for me to pull parts and do analysis/review.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.