2018-07-14 6:27 PM
Hi every body,
I'm doing 1 menu icon (3-4 icon), using icon view widget.
From .png image file to convert .dta, using BmpCvtST.exe in folder STemWin/software in stm32f7cube.
If using image widget, .png files showed ok.
If
using
iconviewwidget, insert stream data .dta, show data have problem, only rectangle blue.
Below is picture that is show problem!
Can you tell me to fix that bug?
Have any other solution to do menu icon?
Thanks.
2018-07-14 8:14 PM
I have just refer link:
https://forum.segger.com/index.php/Thread/1777-GuiBuilder-and-IconView-Problem/
But haven't information to fix that bug!
2018-07-15 2:16 AM
Dear every body,
I have just checked STemWin version.
Current
STemWin version which i'm using is 5.32.
If change to STemWin version 5.40,icon view
insert stream data .dta, show data ok.
But build project after change stemwin to 5.40 have error:
.\Objects\cnc_4axis.axf: error: L6002U: Could not open file .\Src\STemWin\Lib\STemWin532_CM7_OS_Keil_ot.lib: No such file or directory
How to change lib STemWin532_CM7_OS_Keil_ot.lib to STemWin540_CM7_OS_Keil_ot.lib?
Thanks!
2018-07-15 2:47 PM
CubeMX 4.26 use STemWin 5.40
2018-07-16 6:15 AM
Hello
Cong.Tran_Minh
,Please update
to use the latest version V1.0 with upgrade to use SEGGER emWin version V5.You will findSTemWin540_CM7_OS_Keil_ot.libin the folder STM32Cube_FW_F7_V1.0\Middlewares\ST\STemWin\Lib\
With Regards,
Imen
2018-08-08 11:15 PM
Dear you,
I have a problems:
I can read id selected from ICONVIEW_GetSel(), but not set selected id via ICONVIEW_SetSel().
ICONVIEW_SetSel() can't effect?
Can you tellme to fix that bug, please?
Thanks.
Details:
icon_idx = ICONVIEW_GetSel(hIcones);//can get id normally id:0->7, i have 8 icon image.
printf("icon up %d\r\n", icon_idx);
if (icon_idx < icon_idx_max) {
icon_idx++;
}
if (icon_idx >= icon_idx_max) {
icon_idx = icon_idx_max - 1;
}
ICONVIEW_SetSel(hIcones, icon_idx);//haven't effect?
2018-08-08 11:16 PM
About ICONVIEW_SetSel():
2018-08-08 11:18 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.