2016-03-08 8:11 AM
I tried importing the IAR example (STM32-P405) using the eclipse plug-in but was unsuccessful, I kept getting an exception. I don't remember exactly what the exception.
So then I duplicated the project in Eclipse. I was careful to include all of the libraries and get all of the settings to match. Now I am able to compile but unable to link. It's complaining about missing definitions. I've followed the includes through the code and I don't see any reason why those would not be included. As far as I can tell they are included... but I don't see them building. It's complaining about things in the STM32F4xx_StdPeriph_driver/inc directory. It didn't occur to me those wern't even building until just now. I'll look to see why they aren't building. #know-your-tools2016-03-08 8:14 AM
It's complaining about things in the STM32F4xx_StdPeriph_driver/inc directory.
Review Include Paths passed to the compilerReview the Defines passed to the compilerThese may be things stored in the project settings or metadata2016-03-08 10:31 AM
IAR creates the workspace in a subdir of the project but depends on some things in the parent directory to be built. I created the Eclipse project in the same subdir so all the necessary libraries were excluded from the build. I moved the whole project up a directory and after a significant amount of fighting I was able to get it to build.
I sure with the import function worked.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.