2024-12-05 7:36 PM
Hi STM,
I'm working on coding I2S read/write at the same time with STM32F429IGT6.
I enable I2S write with HAL_I2S_Transmit_DMA and Audio playback successfully.
I could also scope the signal from the Sdout pin.
However, if I enable I2S read with HAL_I2S_Receiver_DMA at the same time.
The RX_flag will always show up Busy and play back also can't work.
Do you have the sample code for the I2S read/write at the same time?
2024-12-08 5:47 PM
Hi Team,
This application is for audio echo cancellation.
I used I2S SDIN and SDOUT with the same clock(BCLK and LRCLK).
The TX_DMA is working and Playback on amp is normally.
I could also scope the data output from SDOUT of audio amp.
But RX_DMA can't work correctly.
Do you have the sample code for the it?
2024-12-09 4:47 AM
Hello @ChenkaiYi ,
Check the buffer size and make sure that the DMA data width is set to "Word".
You can try I2S example within STM32CubeF4 package:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.