2016-04-14 7:31 AM
Hello ,
I have configured I2S3ext of STM32F4 which is interfaced with audio codec. In our environment , Sample Frequency is @ 8 KHz . CHSIDE bit of I2S status register always remains in reset state . I have checked no overrun flag has not been set . What could be the other reason for not setting this CHSIDE bit ?- Pinkesh
#i2s-channel-side-issue2016-04-14 8:27 AM
> I have configured I2S3ext
Transmitter or receiver? Which mode? Post perhaps the I2S3ext registers' content. Which pins are you using for I2S3/ext? JW2016-04-14 11:20 PM
Hi Jan,
In our environment , PC11 - I2S3ext _SD line PC12 - I2S3_SD line PC10 - I2S3_CK PA15 - I2S3_WS line I2S3 as full duplex in which I2Sext configured as Slave receiver & I2S as Slave Transmitter while external device work as I2S master . After configuring I2S, SPI3 Peripheral contents are CR2 - 0x80 SR - 0x02 I2SCFGR - 0xC00 I2S3ext Peripheral Contents are CR2 - 0x40 SR - 0x02 I2SCFGR - 0xD00 - PinkeshWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.