2012-11-22 4:53 AM
Hello,
I have fully working I2S with external codec (TLV320AIC23). I have decided to save a crystal and feed the clock to the codec from the I2C pll. So according to the codec pdf this clock needs to be constant (say 12.288 Mhz) and sampling rate is changed via SPI/I2C command. Then the STM32 pdf says that the I2S output clock is based on the sampling rate (256 * Fs). In practice changing the sampling rate when making init of the I2S will change the divider values and correct clock will be available only at 48 kHz. With 8 kHz sampling rate the clock will drop as low as 2 Mhz. Because i thought that would be good idea to have variable sampling rate for different modes of operation i just did a quick hack by setting the dividers const at any rate to output close to 12.288 Mhz. But then i guess the I2S hardware will not function correctly - when i run my software implemented DDS process to output a sine wave (0-4000 Hz) i need to setup sampling frequency of 48 kHz as input of the frequency formula while the codec is running at 8 kHz. So it seems i need to set I2S hardware to run at correct sampling rate and same time have constant output clock to feed the codec. Is this mode of operation possible or i do the whole thing in a wrong way. Any help to clear my confusion will be appreciated. Thanks Regards, Chris2012-11-22 6:05 AM
If I didn't need to use USB I'd definitely consider running the STM32 from the 12.288 MHz crystal, or one of the other magic values for audio.
The AIC23 had a USB as I recall, but I'm not sure that helps given the inflexibly poor divider strategy employed by ST.2012-11-22 6:34 AM
You don't mention which STM32 device you are using, but on STM32F4xx the output of I2S PLL can be directed to the MCO2 output (through its dedicated divider).
It would also help if you would pay more attention to describing your case. Replacing ''I2S'' randomly by ''I2C'' indicates you might not really want anybody to study the details of your problem. JW2012-11-22 6:58 AM
Hi,
Thanks for your responses. clive1: At the moment i have the codec, LCD via software SPI (needs 9bit frames) and PHY in RMII mode(i plan to supply it with 25 Mhz too). So no USB right now, but i think i will try to add USB in near future. waclawek.jan: I am sorry, just a typing error, fixed now. My part is STM32F407 on STM32F4Discovery board. Would redirecting the I2S PLL fix the variable rate based on sampling rate ? Or just output to different pin ? Some more explanation. The reason i need as less possible crystals/oscillators on the final board is because my project is software defined radio. As it requires to be very sensitive by design, it also picks up all the different clocks and this is a big problem. One interesting side effect on the off the shelf Discovery board is the 2 chips with own, 8 Mhz crystal. As temperature changes both crystals move up and down, but with different rate, the sum and difference create interesting 'beat tone' that can be heard on many bands. Back to the I2S - my main confusion is why the I2S output clock changes based on sampling rate ? What part would need such changing clock - some ADC/DACs ? Is it wrong to use this pin as master clock for a CODEC ? BR2012-11-22 7:32 AM
One interesting side effect on the off the shelf Discovery board is the 2 chips with own,
8 Mhz crystal. As temperature changes both crystals move up and down, but with different rate, the sum and difference create interesting 'beat tone' that can be heard on many bands.
Something you'll see pretty much with any pair of independent sources to a varying degree, thus having a single source and some DDS/NCO type frequency generators would have been so much more useful than binary divider chains.
2012-11-22 8:07 AM
> I am sorry, just a typing error, fixed now.
Not completely... ;) > Would redirecting the I2S PLL fix the variable > rate based on sampling rate ? I recommend thorough reading of the relevant chapters of manual(s) (including the RCC chapter) before asking further questions. Also, above I did not say ''*re*direct''; I said ''direct''. You can output the I2SPLL to MCO2 independently from the I2S module (and optionally divide it too). The same clock is then fed to the I2S module and divided by its divider as wished. I don't know if this fits your requirements, as I still don't understand what do you intend to achieve.JW
2012-11-22 9:01 AM
Hi,
The SPI/I2C part in the first post is about the control interface of the codec that is independent of the I2S interface. In normal configuration the codec will run on external crystal (eg 12.288 Mhz) and internally will divide it to achieve sampling rate, which is in turn programmed via the control interface. So i assume the variable I2S rate on the STM32 chip is to accommodate ADC/DACs that don't have such internal logic. Thanks for the suggestion, i will read further and experiment. BR2012-11-22 1:32 PM
Hi JW,
That actually did the trick. Thanks! Now the output clock is constant and not dependent on the I2S sampling rate, also the I2S hardware functions correctly as expected for other than 48 kHz selected rate. I have tested my SoftDDS routine - it can output correct audio signal at any sample rate. Also the constant firing rate of the I2S DMA interrupt is now different, based on the selected sample rate. So for future reference, my settings: HSE clock = 25 Mhz PLL_M = 25 PLLI2S_N = 258 PLLI2S_R = 7 I2SCLK = 36.8571 Mhz (ideal: 36.864 Mhz) Error = 0.0186 MCO2 divider = 3 and init code: ... I2S_InitStructure.I2S_MCLKOutput = I2S_MCLKOutput_Disable; ... // Configure MCO2 (PC9) GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOC, &GPIO_InitStructure); // Output I2S PLL via MCO2 pin - 12.288 Mhz RCC_MCO2Config(RCC_MCO2Source_PLLI2SCLK, RCC_MCO2Div_3); Regards, ChrisWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.