2024-05-07 6:40 PM
Hi,
now I'm implementing i2c with 1 master(U575ZI-Q) and 3 slave(L432KC) boards.
master transmit dataBuf to slave
HAL_I2C_Master_Transmit_IT(&hi2c1, addr<<1, dataBuf, sizeof(dataBuf));
and Slave receive it.
HAL_I2C_Slave_Receive_IT(&hi2c1, dataBuf, sizeof(dataBuf));
I already checked slave address and dataBuf, no problem.
also My code worked well before I change some setting :(
The problem is..
Master is ready to transmit(write) to slave 0x08, but it doesn't transmit the dataBuf contents.
SCL stay LOW and SDA stay HIGH...
IDK what's the problem.
thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.