2015-07-10 2:17 AM
Hallo Every One
I try To Communicate with PCA 9539 PORT EXPANDERand Here Are My Code &sharpdefine slave_add 0x74uint8_t mem[10];/* USER CODE BEGIN Includes *//* USER CODE END Includes *//* Private variables ---------------------------------------------------------*/I2C_HandleTypeDef hi2c1;/* USER CODE BEGIN PV *//* USER CODE END PV *//* Private function prototypes -----------------------------------------------*/void SystemClock_Config(void);static void MX_GPIO_Init(void);static void MX_I2C1_Init(void);/* USER CODE BEGIN PFP *//* USER CODE END PFP *//* USER CODE BEGIN 0 *//* USER CODE END 0 */int main(void){ /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration----------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_I2C1_Init(); /* USER CODE BEGIN 2 */ mem[0]=0x02; mem[1]=255; mem[2]=255; mem[3]=0; mem[4]=0; mem[5]=0; mem[6]=0; mem[7]=1; /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5); HAL_Delay(500); HAL_I2C_Master_Transmit(&hi2c1,slave_add,mem,6,1); /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */}/** System Clock Configuration*/void SystemClock_Config(void){ RCC_OscInitTypeDef RCC_OscInitStruct; RCC_ClkInitTypeDef RCC_ClkInitStruct; __PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2); RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = 16; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 216; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV6; RCC_OscInitStruct.PLL.PLLQ = 4; HAL_RCC_OscConfig(&RCC_OscInitStruct); RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2); HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000); HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);}/* I2C1 init function */void MX_I2C1_Init(void){ hi2c1.Instance = I2C1; hi2c1.Init.ClockSpeed = 100000; hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2; hi2c1.Init.OwnAddress1 = 0; hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLED; hi2c1.Init.OwnAddress2 = 0; hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLED; hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLED; HAL_I2C_Init(&hi2c1);}/** Configure pins as * Analog * Input * Output * EVENT_OUT * EXTI*/void MX_GPIO_Init(void){ GPIO_InitTypeDef GPIO_InitStruct; /* GPIO Ports Clock Enable */ __GPIOA_CLK_ENABLE(); __GPIOB_CLK_ENABLE(); /*Configure GPIO pin : PA5 */ GPIO_InitStruct.Pin = GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);}and Is not working at all Please Help ME Best Regards Herru S #i2c2015-07-13 2:21 AM
Hi setiawan.herru,
1- Please try to use the ''Format Code Block'' feature (left top) so that your code becomes easier to read and to help you.2- I don't see the I2C clock enabled in your code.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.