2008-04-30 5:15 AM
I2C using DMA
2011-05-17 3:34 AM
HI
I wrote code to read ann eeprom using DMA. It works when you call the first time. The problem seems to be after generating a STOP condition. The BUSY flag never goes to 0 when using DMA after a STOP condition. Any idea ?2011-05-17 3:34 AM
Problem solved. For those interested in the code :
#define EEPROM_ADDRESS 0xA0 /* Reads ''len'' bytes from EEPROM starting at address ''addr'' and transfer to ram pointed by ''buffer'' */ s16 rd_i2c_dma_n(I2C_TypeDef *I2C, u8* buffer, u16 addr, u16 len) { u8 device_addr = (EEPROM_ADDRESS | addr >> 7) & 0xfe; DMA_Channel7->CCR = 0; DMA->IFCR |= ((u32)0x0F000000); DMA_Channel7->CCR = (DMA_Channel6->CCR & 0xFFFF800F) | DMA_DIR_PeripheralSRC | DMA_Mode_Normal | DMA_PeripheralInc_Disable | DMA_MemoryInc_Enable | DMA_MemoryDataSize_Byte | DMA_MemoryDataSize_Byte | DMA_Priority_VeryHigh | DMA_M2M_Disable; DMA_Channel7->CNDTR = len; DMA_Channel7->CPAR = (u32) (u32) &I2C->DR; DMA_Channel7->CMAR = (u32) buffer; I2C->CR1 |= (1< while(!check_event(I2C, 0x00030001)); I2C->CR1 |= (1< I2C->DR = device_addr; while(!check_event(I2C, 0x00070082)); I2C->DR = addr; while(!check_event(I2C, 0x00070084)); I2C->CR1 |= (1< while(!check_event(I2C, 0x00030001)); I2C->DR = device_addr | 1; while(!check_event(I2C, 0x00030002)); I2C->CR2 |= (1< DMA_Channel7->CCR |= 1; while(!(DMA->ISR & 0x02000000)); I2C->CR1 |= (1< while(!check_event(I2C, 0x00000000))(void) I2C->DR; return 0; } static u32 check_event(I2C_TypeDef* I2C, u32 I2C_EVENT) { return (I2C->SR1 | (I2C->SR2 << 16)) == I2C_EVENT; } [ This message was edited by: viktor2 on 30-04-2008 17:56 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.