2017-09-20 2:18 AM
Hello,
I'm having trouble using I2C (Fast Mode, Master Mode) on a STM32F411RE (Nucleo-F411RE).
My code gets stuck after sending the I2C Address here:
while (!(I2C1->SR1 & I2C_SR1_ADDR));
On the bus I get short pulses, but no clock signal or data on SDA.
My full code is this:
//I2C configuration
void I2C_Config(void){ RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; //enable AHB1 GPIO->B clock RCC->APB1ENR |= RCC_APB1ENR_I2C1EN; //enable Clock for I2C GPIOB->AFR[1] |= (1 << 2) | (1 << 6); //AF4 GPIOB->MODER |= GPIO_MODER_MODER8_1 | GPIO_MODER_MODER9_1; //set PB8 & PB9 to alternate function GPIOB->OTYPER |= GPIO_OTYPER_OT_8 | GPIO_OTYPER_OT_9; //Open-Drain configuration for PB8 & PB9, Reset configuration ///GPIOB->PUPDR |= GPIO_PUPDR_PUPDR8_0 | GPIO_PUPDR_PUPDR9_0; //External Pull-up's GPIOB->OSPEEDR &= ~(GPIO_OSPEEDER_OSPEEDR8_0 & GPIO_OSPEEDER_OSPEEDR9_0); I2C1->CR1 |= I2C_CR1_SWRST; I2C1->CR1 &= ~(I2C_CR1_SWRST); I2C1->CR2 &= ~(I2C_CR2_FREQ); //reset Frequency I2C1->CR2 |= 30; //30MHz from APB1 I2C1->CCR &= ~I2C_CCR_CCR; I2C1->CCR |= I2C_CCR_FS | I2C_CCR_DUTY | 3; I2C1->TRISE |= 1 << 1 | 1 << 3; I2C1->CR1 |= I2C_CR1_PE | I2C_CR1_ACK;}//Start I2C Communicationvoid I2C_Start(void){ I2C1->CR1 |= I2C_CR1_START; while (!(I2C1->SR1 & I2C_SR1_SB));}//Stop I2C Communicationvoid I2C_Stop(void){ I2C1->CR1 |= I2C_CR1_STOP;}//Send I2C Slave Addressvoid I2C_ADDR(unsigned char ADDR){ char clear_addr_flag; I2C1->DR = ADDR; //Write I2C Slave Address while (!(I2C1->SR1 & I2C_SR1_ADDR)); //Wait till Address is sent clear_addr_flag = (I2C1->SR2); //Reset ADDR-Flag}//Write Data (Byte) to I2C Busvoid I2C_Write(unsigned char write_data){ I2C1->DR = write_data; while (!(I2C1->SR1 & I2C_SR1_TXE));}//Read Data from I2C Bus, Acknoledge Bit=> I2C_ACKDunsigned char I2C_Read(void){ while (!(I2C1->SR1 & I2C_SR1_RXNE)); return (I2C1->DR);}Can someone tell me why the ADDR Bit is not set?
Thank you
#i2c #nucleo ##stm32f411re #stm32f42017-09-21 2:53 AM
Hi,
I'm really hoping someone can help me...!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.