2012-10-28 9:18 AM
I am trying to write an i2c driver for my stm32f100 discovery board. To verify that it is setup right, I want to send a start condition and check to see that the SDA line goes low while SCL stays high. I have the following code (borrowed from the web)...
void I2C_Setup(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
I2C_InitTypeDef I2C_InitStructure;
/* I2C1 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);
/*enable I2C*/
I2C_Cmd(I2C1,ENABLE);
/* I2C1 SDA and SCL configuration */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD; // Alternate function Open Drain
GPIO_Init(GPIOB, &GPIO_InitStructure);
/*SCL is pin06 and SDA is pin 07 for I2C1*/
/* I2C1 configuration */
I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;
I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;
I2C_InitStructure.I2C_OwnAddress1 = 0x04;
I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;
I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;
I2C_InitStructure.I2C_ClockSpeed = I2C_SPEED ;
I2C_Init(I2C1, &I2C_InitStructure);
}
I call this function first and then try to send the start condition...
/* initiate start sequence */
I2C_GenerateSTART(I2C1, ENABLE);
/* check start bit flag */
while(!I2C_GetFlagStatus(I2C1, I2C_FLAG_SB));
I have an o-scope connected to both SDA and SCL but I don't see SDA go low as I would expect. I just put in the own address as 0x4 for now.
There is no slave on the bus, I just have the two gpio lines going to a breadboard fed by 3.3 from the discovery board and those pins are pulled high with 4.7K pullups. I was expecting to see SDA go low.
Is my understanding of the protocol incorrect or is the web sample missing something?
2012-10-28 1:13 PM
Have you enabled the GPIOB clock?
2012-10-28 2:34 PM
No, I didn't enable the GPIOB clock. That was it. It was left out of the sample I took from the web.
thanks clive1!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.