2017-03-20 10:24 AM
Going through HAL code, I see this
static HAL_StatusTypeDef I2C_SlaveTransmit_TXE(I2C_HandleTypeDef *hi2c)
{ /* Declaration of temporary variables to prevent undefined behavior of volatile usage */ uint32_t CurrentState = hi2c->State;if(hi2c->XferCount != 0U)
{ /* Write data to DR */ hi2c->Instance->DR = (*hi2c->pBuffPtr++); hi2c->XferCount--;if((hi2c->XferCount == 0U) && (CurrentState == HAL_I2C_STATE_BUSY_TX_LISTEN))
{ /* Last Byte is received, disable Interrupt */ __HAL_I2C_DISABLE_IT(hi2c, I2C_IT_BUF); /* Set state at HAL_I2C_STATE_LISTEN */ hi2c->PreviousState = I2C_STATE_SLAVE_BUSY_TX; hi2c->State = HAL_I2C_STATE_LISTEN; /* Call the Tx complete callback to inform upper layer of the end of receive process */ HAL_I2C_SlaveTxCpltCallback(hi2c); } } return HAL_OK;I am not sure how this approaches the problem with multiple bytes. Since it is just 'if statements', wouldn't that mean I would need it an interrupt to occur for each byte?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.