2014-04-27 10:56 AM
Hi I'
m working on STM32F401 disco EVB with the
Standard Peripherals Library
,
Where i can find a working example on I2C slave?
2014-05-01 11:33 AM
I would also like to see a I2C example from ST Micro. Not one with DMA, not one that is board to board just one that is some type of eval board to a memory device or a ADC or something like that. I've seen some with the STM32Cube but it is so hard to figure out what is going on.
Mike2014-05-04 6:43 PM
You can download STM32F4xx_DSP_StdPeriph_Lib_V1.3.0 here:
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257901
Mike2014-05-05 2:14 PM
Yay! I've got this working pretty well. My biggest problem was that the address of the sensor is x48 and I know it is 7 bit but I did not realize that it needs to be left justified before I call I2C_Send7bitAddress. So, I need to send a x90.
My last remaining problem is that the register I'm reading is 16 bit and I can't quite figure out how to use the std periph library functions to clock in that second byte. I don't need to send the bus address again or the register address, just need to clock in 8 more bits.Code looks like this after it gets the high byte. /* Receive high byte of Data */ data_high = I2C_ReceiveData(I2C1); // Read low byte of Data /* Prepare an NACK for the next data received */ I2C_AcknowledgeConfig(I2C1, DISABLE); /* Test on I2C1 EV7 and clear it */ timeout = ADT7410_TIMEOUT_MAX; /* Initialize timeout value */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED)) { /* If the timeout delay is exeeded, exit with error code */ if ((timeout--) == 0) { return ERROR; } } /* Receive the Data */ data_low = I2C_ReceiveData(I2C1); // Build 16 bit data word *read_data = (uint16_t) data_high; *read_data <<= 8; *read_data += (uint16_t) data_low; I2C_GenerateSTOP(I2C1, ENABLE); /* return the read data */ return SUCCESS; but it times out and I don't see that second transfer on the scope so I must not be calling I2C_CheckEvent correctly or something like that.I'd appreciate any ideas.MikeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.