2008-07-09 4:51 AM
I2C read from memory problem
2011-05-17 3:25 AM
Hello I dont get my code to work for reading from the M24 series memory. I got a 64kb version.
This is my write code and I think its working but I dont know, becuse I cant read from the memory to verify that. void I2C_EE_ByteWrite(u8* pBuffer, u8 WriteAddr) { /* Send STRAT condition */ I2C_GenerateSTART(I2C1, ENABLE); /* Test on EV5 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); /* Send EEPROM address for write */ I2C_Send7bitAddress(I2C1, EEPROM_ADDRESS, I2C_Direction_Transmitter); /* Test on EV6 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); // send adress 2 times manual says so /* Send the EEPROM's internal address to write to */ I2C_SendData(I2C1, WriteAddr); /* Test on EV8 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /* Send the EEPROM's internal address to write to */ I2C_SendData(I2C1, WriteAddr); /* Test on EV8 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /* Send the byte to be written */ I2C_SendData(I2C1, *pBuffer); /* Test on EV8 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /* Send STOP condition */ I2C_GenerateSTOP(I2C1, ENABLE); } For reading from the memory I dont really have a clue, but this is my code and it doesnt work. Trying to read 1 byte, I want to read more bytes later but im trying just to read one byte right now. /* ByteRead code */ void I2C_EE_ByteRead(u8* pBuffer, u8 ReadAddr) { // Check busy flag (dont know if I need that but just in case maybe) I2C_CheckEvent(I2C1, I2C_FLAG_BUSY); // Start I2C_GenerateSTART(I2C1, ENABLE); // Test EV5 while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); // Send device adress should it be A0 here or A1? I have no cables to the chip enable E0,E1,E2 ports. I2C_Send7bitAddress(I2C1, 0xA0, I2C_Direction_Transmitter); // Test EV6 while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); // Clear EV6 by setting again the PE bit I2C_Cmd(I2C1, ENABLE); // Send address for reading I2C_SendData(I2C1, 0x1); // Test EV8 while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); // Send address for reading I2C_SendData(I2C1, 0x1); // Test EV8 while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); // Start I2C_GenerateSTART(I2C1, ENABLE); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(I2C1, 0xA1, I2C_Direction_Receiver); // Inactive ACK I2C_AcknowledgeConfig(I2C1, DISABLE); // I doesnt go in there, what should I do here? if(I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED)) { *pBuffer = I2C_ReceiveData(I2C1); } // Stop I2C_GenerateSTOP(I2C1, ENABLE); I2C_AcknowledgeConfig(I2C1, DISABLE); } Please help me im getting gray hair on this one :-[2011-05-17 3:25 AM
hello ppl!
Now it works fine, I found some errors in the code ;)2011-05-17 3:25 AM
Can u post corrected code?
2011-05-17 3:25 AM
Quote:
On 26-02-2008 at 16:57, larsahl wrote: // send adress 2 times manual says so /* Send the EEPROM's internal address to write to */ I2C_SendData(I2C1, WriteAddr); /* Test on EV8 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /* Send the EEPROM's internal address to write to */ I2C_SendData(I2C1, WriteAddr); /* Test on EV8 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); Where in the manual it said that you have to sennd the address twice???We’re moving the ST Community to a new platform to give you a better and more reliable community experience.