2015-03-21 8:51 AM
Hi, I' am trying to let STM32f072b discovery board to communicate with my I2C device(TSL2561T).
But I'm having problem in that which I don't know why the code is not working. I know where it stops (marked with orange color). And please point out any mistake in my code. Here's my code.&sharpdefine IIC_SDA_PIN GPIO_Pin_11
&sharpdefine IIC_SCL_PIN GPIO_Pin_10
&sharpdefine IIC_GPIO GPIOB
&sharpdefine IIC_SDA_PS GPIO_PinSource11
&sharpdefine IIC_SCL_PS GPIO_PinSource10
&sharpdefine IIC_PIN_AF GPIO_AF_1
&sharpdefine TSL2561_Add 0x39 //Slave addr � also 0x29 or 0x49
&sharpdefine TIMING 0x81
&sharpdefine Control 0x80
&sharpdefine powerup 0x03
&sharpdefine DATA0LOW 0x8C
&sharpdefine DATA0HIGH 0x8D
&sharpdefine DATA1LOW 0x8E
&sharpdefine DATA1HIGH 0x8F
&sharpdefine LED1_Pin GPIO_Pin_9
&sharpdefine LED2_Pin GPIO_Pin_8
&sharpdefine LED3_Pin GPIO_Pin_7
&sharpdefine LED4_Pin GPIO_Pin_6
&sharpdefine LED_GPIO GPIOC
&sharpdefine uchar unsigned char
uchar DataLow0,DataHigh0,DataLow1,DataHigh1,Channel0,Channel1;
uint32_t E;
void IIC_init(void)
{
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB,ENABLE );
RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2, ENABLE);
GPIO_PinAFConfig(IIC_GPIO, IIC_SCL_PS, GPIO_AF_1); // SCL
GPIO_PinAFConfig(IIC_GPIO, IIC_SDA_PS, GPIO_AF_1); //SDA
//Configure pins: SCL and SDA ------------------
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.GPIO_Pin = IIC_SDA_PIN | IIC_SCL_PIN;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_Level_1;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;
//GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStruct.GPIO_OType = GPIO_OType_OD;
GPIO_Init(GPIOB, &GPIO_InitStruct);
I2C_InitTypeDef I2C_InitStruct;
I2C_InitStruct.I2C_Timing = 0x00001010;
I2C_InitStruct.I2C_AnalogFilter = I2C_AnalogFilter_Enable;
I2C_InitStruct.I2C_OwnAddress1 = 0x08;
I2C_InitStruct.I2C_Mode = I2C_Mode_I2C;
I2C_InitStruct.I2C_Ack = I2C_Ack_Enable;
I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;
I2C_Init(I2C2, &I2C_InitStruct);
I2C_Cmd(I2C2, ENABLE);
}
void IIC_write(uint8_t I2C_Register, uint8_t Val)
{
while(I2C_GetFlagStatus(I2C2, I2C_FLAG_BUSY) == SET);
I2C_TransferHandling( I2C2, TSL2561_Add, 1, I2C_Reload_Mode, I2C_Generate_Start_Write);
//Ensure the transmit interrupted flag is set
while(I2C_GetFlagStatus(I2C2, I2C_FLAG_TXIS) == RESET);
//Send the register address we wish to write to
GPIO_SetBits(LED_GPIO,LED3_Pin);
I2C_SendData(I2C2, I2C_Register);
while(I2C_GetFlagStatus(I2C2, I2C_FLAG_TCR) == RESET);
I2C_TransferHandling(I2C2, TSL2561_Add, 1, I2C_AutoEnd_Mode, I2C_No_StartStop);
while(I2C_GetFlagStatus(I2C2, I2C_FLAG_TXIS) == RESET);
I2C_SendData(I2C2, Val);
while(I2C_GetFlagStatus(I2C2, I2C_FLAG_STOPF) == RESET);
I2C_ClearFlag(I2C2, I2C_FLAG_STOPF);
}
uint32_t IIC_read(I2C_TypeDef* I2Cx, uint8_t I2C_Register)
{
int8_t SingleData = 0;
while(I2C_GetFlagStatus(I2C2, I2C_FLAG_BUSY) == SET);
I2C_TransferHandling(I2C2, TSL2561_Add, 1, I2C_SoftEnd_Mode, I2C_Generate_Start_Write);
while(I2C_GetFlagStatus(I2C2, I2C_FLAG_TXIS) == RESET);
I2C_SendData(I2C2, I2C_Register);
while(I2C_GetFlagStatus(I2C2, I2C_FLAG_TC) == RESET);
I2C_TransferHandling(I2C2, TSL2561_Add, 1 , I2C_AutoEnd_Mode, I2C_Generate_Start_Read);
while(I2C_GetFlagStatus(I2C2, I2C_FLAG_RXNE) == RESET);
SingleData = I2C_ReceiveData(I2C2);
while(I2C_GetFlagStatus(I2C2, I2C_FLAG_STOPF) == RESET);
I2C_ClearFlag(I2C2, I2C_FLAG_STOPF);
return SingleData;
}
void LED_init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,ENABLE);
GPIO_InitStruct.GPIO_Pin =LED1_Pin | LED3_Pin |LED2_Pin | LED4_Pin;
GPIO_InitStruct.GPIO_Mode =GPIO_Mode_OUT;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_Level_2;
GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOC , &GPIO_InitStruct);
}
int main(void)
{
SystemInit();
SystemCoreClockUpdate();
SysTick_Config(SystemCoreClock/MillisecondsIT);
IIC_init();
LED_init();
GPIO_SetBits(LED_GPIO,LED2_Pin);
E=0;
IIC_write(Control, powerup);
DelayMil(10);
while(1)
{
DataLow0 = IIC_read(I2C2, DATA0LOW);
DataHigh0 = IIC_read(I2C2,DATA0HIGH);
Channel0 = 256*DataHigh0 + DataLow0;
DataLow1 = IIC_read(I2C2,DATA1LOW);
DataHigh1 = IIC_read(I2C2,DATA1HIGH);
Channel1 = 256*DataHigh1 + DataLow1;
DelayMil(100);
{
//Calculating Lux
if(0.0< Channel1/Channel0 && Channel1/Channel0 <=0.50)
E=(0.0304*Channel0-0.062*Channel0*pow(Channel1/Channel0, 1.4));
if(0.50<Channel1/Channel0&&Channel1/Channel0<=0.61)
E=(0.0224*Channel0-0.031*Channel1);
if(0.61<Channel1/Channel0&&Channel1/Channel0<=0.80)
E=(0.0128*Channel0-0.0153*Channel1);
if(0.80<Channel1/Channel0&&Channel1/Channel0<=1.30)
E=(0.00146*Channel0-0.00112*Channel1);
if(Channel1/Channel0>1.30)
E=0;
}
if (E>1)
{
DelaySec(1);
GPIO_SetBits(LED_GPIO,LED1_Pin);
}
else
GPIO_ResetBits(LED_GPIO,LED1_Pin);
}
} #i2c-stm32f072b
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.