2015-10-14 6:35 AM
hi,
I am trying to input capture and output compare values but i cant able to read those values is there any mistake in my code.I enabled clocks also.But still I am getting this issue.Can any one guide me please.// init function void MX_TIM15_Init(void){ TIM_MasterConfigTypeDef sMasterConfig; TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig; TIM_IC_InitTypeDef sConfigIC; TIM_OC_InitTypeDef sConfigOC; htim15.Instance = TIM15; htim15.Init.Prescaler = 0; htim15.Init.CounterMode = TIM_COUNTERMODE_UP; htim15.Init.Period = 16666; htim15.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim15.Init.RepetitionCounter = 0; HAL_TIM_IC_Init(&htim15); HAL_TIM_OC_Init(&htim15); sMasterConfig.MasterOutputTrigger = TIM_TRGO_ENABLE; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; HAL_TIMEx_MasterConfigSynchronization(&htim15, &sMasterConfig); sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE; sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF; sBreakDeadTimeConfig.DeadTime = 0; sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE; sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH; sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE; HAL_TIMEx_ConfigBreakDeadTime(&htim15, &sBreakDeadTimeConfig); sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_FALLING; sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI; sConfigIC.ICPrescaler = TIM_ICPSC_DIV2; sConfigIC.ICFilter = 0; HAL_TIM_IC_ConfigChannel(&htim15, &sConfigIC, TIM_CHANNEL_1); sConfigOC.OCMode = TIM_OCMODE_TIMING; sConfigOC.Pulse = 0; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET; sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET; TIM_OC2_SetConfig( (TIM_TypeDef* )&htim15.Instance,&sConfigOC); HAL_TIM_OC_ConfigChannel(&htim15, &sConfigOC, TIM_CHANNEL_2); HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_2); HAL_TIM_OC_Start_IT(&htim15,TIM_CHANNEL_2); HAL_TIM_IC_Start_IT(&htim15,TIM_CHANNEL_1); __HAL_TIM_ENABLE_IT(&htim15,TIM_IT_CC2); //output compare __HAL_TIM_ENABLE_IT(&htim15,TIM_IT_CC1);}//interrupt functionsvoid HAL_TIM_OC_DelayElapsedCallback(TIM_HandleTypeDef *htim){ uint32_t OutPutCompare = 0;OutPutCompare = HAL_TIM_ReadCapturedValue(&htim15, TIM_CHANNEL_2 ); __HAL_TIM_SET_COUNTER(&htim15,DaliOutPutCompare + 16666 ); __HAL_TIM_CLEAR_IT(&htim15,TIM_IT_CC2); __HAL_TIM_CLEAR_FLAG(&htim15, TIM_FLAG_CC2);}void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){ uint32_t InputCapture;InputCapture = HAL_TIM_ReadCapturedValue(&htim15, TIM_CHANNEL_1 ); __HAL_TIM_SET_COUNTER(&htim15,DaliInputCapture + 16666 ); __HAL_TIM_CLEAR_IT(&htim15,TIM_IT_CC1); __HAL_TIM_CLEAR_FLAG(&htim15, TIM_FLAG_CC1);} #stm32f0-timerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.