2016-04-20 5:06 AM
Hi,
In our environment , we have interfaced codec IC with I2C peripheral . Once codec IC has been configured , both SDA and SCL @ High logic level . Now if controller reset happened , SDA line remains low and inhibits the STM32 start condition . To resolve this, I have written following code . Now if I go for configuring I2C peripheral ,busy flag has been set just after RCC_APB1PeriphClockCmd() API . Any reason behind this ? void ResetI2cLines() { uint8_t i; GPIO_InitTypeDef gpio; // Provid delay before I2c Reset line DelayMS(1); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); // Config SDA and SCL Pin bzero(&gpio, sizeof(gpio)); gpio.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; gpio.GPIO_Mode = GPIO_Mode_OUT; gpio.GPIO_OType = GPIO_OType_PP; gpio.GPIO_PuPd = GPIO_PuPd_UP; gpio.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &gpio); GPIO_SetBits(GPIOB, GPIO_Pin_7); // 9th Pulse NACK signal for(i=0; i<10; i++) { // SCL line Clocking GPIO_SetBits(GPIOB, GPIO_Pin_6); DelayUS(5); GPIO_ResetBits(GPIOB, GPIO_Pin_6); DelayUS(5); } //Stop Signal - SDA Low to High while SCL High GPIO_ResetBits(GPIOB, GPIO_Pin_7); DelayUS(5); GPIO_SetBits(GPIOB, GPIO_Pin_6); DelayUS(2); GPIO_SetBits(GPIOB, GPIO_Pin_7); DelayUS(2); } #i2c #stm32f4 #discovery2016-04-22 11:56 AM
Hi pinkesh,
Make sure that you have well configured the I2C and the SCL & SDA pins (ex: GPIO_Otype = OD) You can refer to the I2C example at this path : stm32f4_dsp_stdperiph_lib\STM32F4xx_DSP_StdPeriph_Lib_V1.6.1\Project\STM32F4xx_StdPeriph_Examples\I2C\I2C_TwoBoards -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.