2018-05-01 7:27 AM
Hi ,
I am migrating from STM32f101 I2C to Stm32f302, the migration document says this is a complete re write of the code . So i used the STM cube to generate the startup code for the I2C for 100khz. I know the board is working and the external component is correct as it is on the same pins. to access the data on the external port expander pca9554 i need to write the slave address +command then read the data by sending the slave address and 8 extra clocks
I am assuming the Hal library is taking care of the start stop and acknowledgements on the i2c bus
I2C acording to cube is setup as follows for 7 bit adress mode
/* I2C1 init function */
void MX_I2C1_Init2(void){hi2c2.Instance = I2C1;
hi2c2.Init.Timing = 0x00901D23; hi2c2.Init.OwnAddress1 = 0; hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c2.Init.OwnAddress2 = 0; hi2c2.Init.OwnAddress2Masks = I2C_OA2_NOMASK; hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE; if (HAL_I2C_Init(&hi2c2) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configure Analogue filter
*/ if (HAL_I2CEx_ConfigAnalogFilter(&hi2c2, I2C_ANALOGFILTER_ENABLE) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configure Digital filter
*/ if (HAL_I2CEx_ConfigDigitalFilter(&hi2c2, 0) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}My reading of the data is a follows slave adress is 0x40 ,
ReadAddr=command byte =0x00
//========================================================================
//// pBuffer: is pointer for data BYTE read back// ReadAddr: contains Command byte of device for reading////============================================================================void read_9554(uint8_t* pBuffer,uint8_t ReadAddr)
{u16 NumByteToRead =0x0001;
u8 slave_adressr=0x00;u8 rxdata=0x00;slave_adressr=DEV_ADDRESS|0x01;//sets last bit in device address byte for reading
while(HAL_I2C_Master_Transmit(&hi2c2, (uint16_t)slave_adressr, (uint8_t*)ReadAddr, 1, 10000)!= HAL_OK)
{ /* Error_Handler() function is called when Timeout error occurs. When Acknowledge failure occurs (Slave don't acknowledge its address) Master restarts communication */ if (HAL_I2C_GetError(&hi2c2) != HAL_I2C_ERROR_AF) { Error_Handler(); }}while(HAL_I2C_Master_Receive(&hi2c2, (uint16_t)slave_adressr, (uint8_t *)pBuffer, 1, 10000) != HAL_OK){ /* Error_Handler() function is called when Timeout error occurs. When Acknowledge failure occurs (Slave don't acknowledge it's address) Master restarts communication */ if (HAL_I2C_GetError(&hi2c2) != HAL_I2C_ERROR_AF) { Error_Handler(); }}i2c_delay(10);
}Every time it get to the wrtie or read function it goes to the hard error function , i can figure out why .
setup is taken from the I2C/I2C_TwoBoards_ComPolling/Src/main.c in the cube repository so it should work but it doesn't.
Could someone please help.
thanks
2018-05-01 7:39 AM
Implement a proper Hard Fault Handler, and look at the instructions (disassembly) and registers at the faulting location.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.