2016-02-02 12:32 PM
hi
I have problem with this function I2C_GetFlagStatus, when I call it as bellow :I2C_GetFlagStatus(IOE_I2C, I2C_FLAG_SB)/**************************************FlagStatus I2C_GetFlagStatus(I2C_TypeDef* I2Cx, uint32_t I2C_FLAG){ FlagStatus bitstatus = RESET; __IO uint32_t i2creg = 0, i2cxbase = 0; /* Check the parameters */ assert_param(IS_I2C_ALL_PERIPH(I2Cx)); assert_param(IS_I2C_GET_FLAG(I2C_FLAG)); /* Get the I2Cx peripheral base address */ i2cxbase = (uint32_t)I2Cx; /* Read flag register index */ i2creg = I2C_FLAG >> 28; /* Get bit[23:0] of the flag */ I2C_FLAG &= FLAG_MASK; if(i2creg != 0) { /* Get the I2Cx SR1 register address */ i2cxbase += 0x14; } else { /* Flag in I2Cx SR2 Register */ I2C_FLAG = (uint32_t)(I2C_FLAG >> 16); /* Get the I2Cx SR2 register address */ i2cxbase += 0x18; } if(((*(__IO uint32_t *)i2cxbase) & I2C_FLAG) != (uint32_t)RESET) { /* I2C_FLAG is set */ bitstatus = SET; } else { /* I2C_FLAG is reset */ bitstatus = RESET; } /* Return the I2C_FLAG status */ return bitstatus;}/**************************************the function returns set bitstatuse but when I call it as bellow:I2C_GetFlagStatus(IOE_I2C, I2C_FLAG_ADDR)the function returns reset bitstatuse! I'm very confused since value of I2C_FLAG_SB is 0x10000001 and value of I2C_FLAG_ADDR is 0x10000002. the program should be return set bitstatuse to work, how can I fix it? #i2c #i2c_getflagstatusWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.