2018-09-16 3:42 PM
Hello, I have a problem to communicate with 24LC02B memory. If I look with the logic analyzer, no data on CLK and DATA pins. Here is my code. What is wrong?
Thank you
#define I2C1_DEVICE_ADDRESS 0x50
#define MEMORY_ADDRESS 0x08
uint8_t xBuffer[1];
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_AFIO_CLK_ENABLE();
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Pin = I2C_SDA_Pin;
HAL_GPIO_Init(I2C_SDA_Port, &GPIO_InitStruct);
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Pin = I2C_SCL_Pin;
HAL_GPIO_Init(I2C_SCL_Port, &GPIO_InitStruct);
I2C_EEPROM.Instance = I2C1;
I2C_EEPROM.Init.ClockSpeed = 100000;
I2C_EEPROM.Init.DutyCycle = I2C_DUTYCYCLE_2;
I2C_EEPROM.Init.OwnAddress1 = 0x00;
I2C_EEPROM.Init.OwnAddress2 = 0x00;
I2C_EEPROM.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
I2C_EEPROM.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
I2C_EEPROM.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
I2C_EEPROM.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if(HAL_I2C_Init(&I2C_EEPROM) != HAL_OK)
{
Error_Handler();
}
__HAL_RCC_I2C1_CLK_ENABLE();
...............
bool EEPROM24XX_IsConnected(void) {
if(HAL_I2C_IsDeviceReady(&I2C_EEPROM,(uint16_t) I2C1_DEVICE_ADDRESS<<1,1,100)==HAL_OK)
return true;
else
return false;
}
bool EEPROM24XX_Save(void) {
xBuffer[0] = 55; // for test only
if(HAL_I2C_Mem_Write(&I2C_EEPROM,(uint16_t) I2C1_DEVICE_ADDRESS<<1,MEMORY_ADDRESS,1,xBuffer,1,100) == HAL_OK) {
HAL_Delay(10);
return true;
}
else return false;
}
bool EEPROM24XX_Load(void) { // should read 55
if(HAL_I2C_Mem_Read(&I2C_EEPROM,(uint16_t) I2C1_DEVICE_ADDRESS<<1,MEMORY_ADDRESS,1,xBuffer,1,100) == HAL_OK) {
return true;
} else return false;
}response of EEPROM24XX_IsConnected os always false, and the same also WRITE function,
Solved! Go to Solution.
2018-09-16 5:09 PM
What STM32 part?
You need to specify the AF mux setting on most STM32 family parts.
GPIO_InitStruct.Alternate = I2Cx_SCL_AF;
And enable the I2C peripheral clock before you initialize the peripheral, synchronous logic sensitive to that.
Inspect the RCC, GPIO and I2C peripheral registers in the debugger to confirm you've got the settings straight.
/* Definition for I2Cx Pins */
#define I2Cx_SCL_PIN GPIO_PIN_8
#define I2Cx_SCL_GPIO_PORT GPIOB
#define I2Cx_SCL_AF GPIO_AF4_I2C1
#define I2Cx_SDA_PIN GPIO_PIN_9
#define I2Cx_SDA_GPIO_PORT GPIOB
#define I2Cx_SDA_AF GPIO_AF4_I2C1
2018-09-16 5:09 PM
What STM32 part?
You need to specify the AF mux setting on most STM32 family parts.
GPIO_InitStruct.Alternate = I2Cx_SCL_AF;
And enable the I2C peripheral clock before you initialize the peripheral, synchronous logic sensitive to that.
Inspect the RCC, GPIO and I2C peripheral registers in the debugger to confirm you've got the settings straight.
/* Definition for I2Cx Pins */
#define I2Cx_SCL_PIN GPIO_PIN_8
#define I2Cx_SCL_GPIO_PORT GPIOB
#define I2Cx_SCL_AF GPIO_AF4_I2C1
#define I2Cx_SDA_PIN GPIO_PIN_9
#define I2Cx_SDA_GPIO_PORT GPIOB
#define I2Cx_SDA_AF GPIO_AF4_I2C1
2018-09-16 9:43 PM
Hi, STM32F103RB. I believe I do not need this here
2018-09-16 10:05 PM
Still going to enable the clock earlier.
2018-09-16 11:45 PM
Now it is just after pin init. No change. Is possible that HAL_I2C_Mem_Read is not compatible with 24LC02B memory? Anyway, still no data on scope during I2C communication.
2018-09-17 12:02 AM
Do you see anything at all with the scope ?
Is the slave address on the bus correct ?
And does the slave ACKnowledge it ?
If nothing at all shows up, the problem is (as Clive pointed out) your initialization.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.