2016-06-07 7:54 AM
Dear All,
I am using CubeMx F4 V1.12.0 I want to use I2C with DMA on the STM32F429 but it is not working. In the stm32f4xx_hal_i2c.c it is noted (+++) Configure the priority and enable the NVIC for the transfer complete interrupt on the DMA Tx or Rx Stream and CubeMx 4.15.0 generates the code for the 2 DMA Interrupts (rx & tx) but the I2C is not working. But in the stm32f4xx_hal_i2c.c I2C_DMAXferCplt() at line 4938 I see these lines /* Enable EVT and ERR interrupt */ __HAL_I2C_ENABLE_IT(hi2c, I2C_IT_EVT | I2C_IT_ERR); So it seems that the 2 I2C Event & Error Interrupts must also be in place to finalize the transmission; Is it right?Thanks for the clarification
2016-06-08 2:37 AM
Hi lecordier.guy.001,
I suggest you to start from I2C examples under the STM32F4 cube firmware package:STM32Cube_FW_F4_V1.12.0\Projects\STM32F429I Discovery\Examples\I2C\I2C_TwoBoards_ComDMAThis example describes how to perform I2C data buffer transmission/reception between two boards, via DMA.-Syrine-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.