2020-01-28 1:23 AM
I am looking a STM board that contains the SPI controller that exercise the ssp_pl022_r1p3 prime cell IP, http://infocenter.arm.com/help/topic/com.arm.doc.ddi0194g/DDI0194G_ssp_pl022_r1p3_trm.pdf.
Thanks for your help for providing the information.
Solved! Go to Solution.
2020-01-28 8:05 AM
Quick googling revealed that the Wiznet (e.g. W7500) and the various NXP LPCxxxx chips contain something which resembles this IP.
JW
2020-01-28 1:39 AM
Why do you think any STM32 would contain that IP?
JW
2020-01-28 5:04 AM
In addition to @Community member's question, Why does it matter what specific IP is used?
Every microcontroller manufacturer documents the operation & behaviour of their peripherals, and provides examples, etc, on how to use them - why is the underlying IP relevant?
2020-01-28 7:27 AM
Yes, it is understood that every micro controller manufacturer have their own peripherals and examples. As like cortex-M4 series is ARM IP and some soc vendors made have soc's, exploring other IP's from ARM to gain more understanding about various SPI IP's.
At present I am working with the STM32F446VE series board. In lieu that exploring the STM boards, incase if any have the specified IP. I dont think it is insane to ask.
2020-01-28 7:36 AM
SPI to a CPU core is an apples-to-oranges comparison.
With the CPU, it does specifically matter - because it defines the entire development toolchain, environment, and ecosystem.
But why is that particular SPI implementation important to you?
Does it do something in particular that you need - and can't find elsewhere?
2020-01-28 8:05 AM
Quick googling revealed that the Wiznet (e.g. W7500) and the various NXP LPCxxxx chips contain something which resembles this IP.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.