2011-05-31 12:38 PM
I want my TIM4 interrupt, interrupt TIM6 ISR ?
with this configuration I cannot --------------------------------------------------------------------- /* Enable the TIM4 gloabal Interrupt */ NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;NVIC_Init(&NVIC_InitStructure);
/* Enable the TIM6 gloabal Interrupt */
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); NVIC_InitStructure.NVIC_IRQChannel = TIM6_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);2011-05-31 2:47 PM
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); is a global setting, set it once, prior to initializing the individual sources.
Your code looks reasonable. What's not happening? Are you initializing the timers properly, what about the service routines? Suggest you create a minimal demo that just does the TIM4 and TIM6 initialization and service routines.2011-06-01 1:06 AM
Hi Clive,
I think that mehmet should use priotity group 1 in order to get the preemption with preemtion priority equal to 0 for TIM4 and equal to 1 for TIM6. I think that using this config TIM4 can preempt (interrupt) TIM6. Isn't it ? Priority group has no preemption priority !!!!2011-06-01 1:33 AM
hello thank you ,
my TIM4 is counting encoder pulses from servo motor I am building an variable named enkoder for position information which is updated in TIM6 ISR which is setup to 1 milisecond period but just during this line enkoder=counterhi+TIM4->CNT;sometimes the TIM4->CNT updates but counterhi is old value and there is about 10000 count difference in enkoder value and the motor gives overcurrent and stops becouse of speed control loop - I catch this with following line if (labs(enkomem-enkoder)>500) enkoder=counterhi+TIM4->CNT;
however still 10000 difference becouse I think TIM4 ISR doesnot interrupt TIM6 ISR this happening every 1 or 2 minutes --------------------------------------------------------------------------- void TIM4_IRQHandler(void){ if(TIM_GetITStatus(TIM4, TIM_IT_Update) == SET){ TIM_ClearFlag(TIM4, TIM_FLAG_Update); TIM_ClearITPendingBit(TIM4, TIM_IT_Update); uint16_t current = TIM4->CNT; if ( current < 5000 ) counterhi += 10000; // Roll over in upwards direction else counterhi -= 10000;// Roll over in downwards direction } --------------------------------------------------------------------------------------------- void TIM6_IRQHandler(void){ TIM_ClearFlag(TIM6, TIM_FLAG_Update); TIM_ClearITPendingBit(TIM6, TIM_IT_Update); enkoder=counterhi+TIM4->CNT; at this point every 1 , 2 minute TIM4->CNT updates but counterhi doesnot if (labs(enkomem-enkoder)>500) enkoder=counterhi+TIM4->CNT; speed = (enkomem-enkoder)*6; enkomem = enkoder; } ---------------------------------------------------------------------------- hello lowpowermcu, can you please type the code sample for your suggestion
2011-06-01 4:20 AM
Ok, so you have a race condition.
So you'll want to have different preemption levels AND take steps to actively identify and mitigate the situation. Personally I might achieve that by giving TIM6 higher priority, storing the prior value of the high count, clearing the TIM4 Update as the last operation (ie AFTER the compare, increment/decrement), and checking the TIM4 update state in TIM62011-10-13 4:33 AM
Hello clive1,
I
want to run
a
servo
using the
STM32
Discovery
,if
you
have a
suggestion
program to
run
the
servo
?or
you have a
simple
code to
run the
servo
on the
STM32
Discovery
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.