2022-05-13 7:27 AM
void usartConfig(){
USART3->CR1=0x00;
//Configurar UE
USART3->CR1|=(1<<13);
//Configurar M=0
USART3->CR1 &=~(1u<<12);
//Configurar STOP (00)=1
USART3->CR2 &=~(1u<<12);
USART3->CR2 &=~(1u<<13);
//Configurar DMAT
USART3->CR3 &=~(1u<<7);
//Configurar baud rate
USART3->BRR = (3<<0) | (104<<4);
//Configurar TE
USART3->CR1|=(1<<3);
/*//Configurar parity
USART3->CR1 &=~(1u<<10);
*/
//Configurar RE
// USART3->CR1|=(1<<2);
}
void senData(uint8_t data){
//Pasar datos
USART3->SR &=~(1u<<6);
USART3->DR =data;
while(!(USART3->SR & (1<<6)));
}
2022-05-13 9:19 AM
Looks a mess, doing multiple RMW on the registers is inefficient.
What STM32 part?
What pins?
Where's the code to enable the UART clock and pins?
void senData(uint8_t data){
while(!(USART3->SR & (1<<7))); // Front test TXE
USART3->DR = data; // Add data when empty
}
2022-05-15 5:57 AM
DMA ?
2022-05-16 6:58 AM
void enableGPIO(){
activarGPIO_RCC_AHB1(3);
definirModoGPIO(GPIOB,10,GPIO_Mode_AF);//TX enviar
definirModoGPIO(GPIOB,11,GPIO_Mode_AF);//RX recibir
//AF7
GPIOB->AFR[1] &=~(1u<<15);
GPIOB->AFR[1] |=(1<<14);
GPIOB->AFR[1] |=(1<<13);
GPIOB->AFR[1] |=(1<<12);
GPIOB->AFR[1] &=~(1u<<11);
GPIOB->AFR[1] |=(1<<10);
GPIOB->AFR[1] |=(1<<9);
GPIOB->AFR[1] |=(1<<8);
//Configurar los puertos
//Max speed
/*GPIOB->OSPEEDR |=(1<<23);
GPIOB->OSPEEDR |=(1<<22);
GPIOB->OSPEEDR |=(1<<21);
GPIOB->OSPEEDR |=(1<<20);*/
// GPIO_PinAFConfig(GPIOB,10,7);
// GPIO_PinAFConfig(GPIOB,11,7);
}
void configureUART(){
enableUSART_RCC_APB1(18);
USART3->CR1=0x00;
//Configurar UE
USART3->CR1|=(1<<13);
//Configurar M=0
USART3->CR1 &=~(1u<<12);
//Configurar STOP (00)=1
USART3->CR2 &=~(1u<<12);
USART3->CR2 &=~(1u<<13);
//Configurar DMAT
USART3->CR3 |=(1<<7);
//Configurar DMAR
USART3->CR3 |=(1<<6);
//Configurar baud rate
USART3->BRR = (3<<0) | (104<<4);
//Configurar TE
USART3->CR1|=(1<<3);
//Configurar RE
USART3->CR1|=(1<<2);
}
2022-05-17 12:37 AM
Not sure if this will help you, but this is how I initialised my USART3 on the STM32L496. I write direct to registers but using the symbols provided to make the code readable/maintainable.
void Init_UART3 (void)
{
// Reset USART3
RCC->APB1RSTR1 |= RCC_APB1RSTR1_USART3RST;
RCC->APB1RSTR1 &= ~RCC_APB1RSTR1_USART3RST;
// Enable USART3 clock
RCC->APB1ENR1 |= RCC_APB1ENR1_USART3EN;
// MUST write BRR before enabling UART
// Set the baud rate
USART3->BRR = (sys_clock_freq/9600);
//USART defaults to:
// - 8 data bits
// - no parity
// - 1 stop bit
// - 16 times oversampling (better for less accurate clocks)
// Enable parity (defaults to even parity)
USART3->CR1 |= USART_CR1_PCE;
// Enable 9 data bits if we want to use parity (ninth bit becomes parity bit)
USART3->CR1 |= USART_CR1_M0;
// Enable the USART
USART3->CR1 |= USART_CR1_UE;
// Enable the transmitter
USART3->CR1 |= USART_CR1_TE;
// Set PC10 to AF7
// AFR[1] = AFRH, AFRH is used for GPIO bits 8..15
// AFR[0] = AFRL, AFRL is used for GPIO bits 0..7
GPIOC->AFR[1] |= (7<<((10-8)*4));
// Make PC10 (TX) alternate function, push-pull output
GPIOC->MODER &= ~GPIO_MODER_MODER10;
GPIOC->MODER |= GPIO_MODER_MODER10_1;
// Set speed to 2 MHz
// GPIOC->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR10_0;
// Enable the receiver
USART3->CR1 |= USART_CR1_RE;
// Set PC11 to AF7
// AFR[1] = AFRH, AFRH is used for GPIO bits 8..15
// AFR[0] = AFRL, AFRL is used for GPIO bits 0..7
GPIOC->AFR[1] |= (7<<((11-8)*4));
// Make PC11 (RX) alternate function
GPIOC->MODER &= ~GPIO_MODER_MODER11;
GPIOC->MODER |= GPIO_MODER_MODER11_1;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.