2019-11-22 3:49 AM
I'm working on a project using STM32F0 discovery board and we bought a TFT LCD from a local distributor, part number TM028HDHG59. The datasheet they sent mentioned it has the driver IC ST7789vi and it has RGB/3-wire SPI interface. Since I'm new to STM32 controller programming, i chose to use SPI interface, because i have experience using SPI in 8-bit controllers.
The issues I'm facing are, not able to find a suitable library file, mainly because the pinout in the datasheet didnt mention a DC pin. I'll attach the picture of the display and its datasheet.
I have asked support from the local distributor, but they can provide support for Renesas controllers only. Changing controllers means I have to spend more time to learn and get used to it and i cant afford the time.
I would appreciate any help provided, Thanks in advance.
2019-11-22 3:58 AM
You might have to write one.
Check the BSP for different Cube repositories, beyond just the F0 series one.
Check with the display/board vendor for example source to use/port.
2019-11-22 4:04 AM
I'm pretty new to STM32 controller. I have only worked with 8-bit controllers, like PIC16F and Arduino Uno. Writing a library is well beyond me. I actually tried though, but i didnt understand much.
Vendor will provide support, but for Renesas controllers only and I cant change controllers now.
I have found some ILI9341 libraries, which i read in the net, is similar to ST7789. But my display doesnt have a DC pin. So I cant use the ILI9341 library, because it uses DC pin.
2019-11-22 4:26 AM
But beyond the specifics of the Renasas SPI interface, presumably most everything else will be the same? You'll need to leverage the materials you can get.
...\STM32Cube\Repository\STM32Cube_FW_F7_V1.15.0\Drivers\BSP\Components\st7789h2
2019-11-22 4:30 AM
Thanks very much. I'll try that out and will update the results here.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.