2022-11-10 9:13 AM
Hello, people.
I have problem using uart on stm32f207ZG, for some reason my board only uses 4 uart and the others don't work. I set everything up as in the example, everything is assembled and flashed, but the UART is silent from 1 to 6 UART, except for 4 UART.
Help.
2022-11-10 9:29 AM
Should we guess what's wrong, or are you going to present this in a manner that can be reviewed or analyzed?
Pins properly assigned and configured?
Correct clocks enabled?
Right pins used?
2022-11-10 10:02 AM
I did everything as in the example and it works for people)), but not for me.
Works only 4 uart.
With the settings, everything hums, it even passed in debugging, everything is zero in the registry.
Is there a bug in the HAL library or is the hardware part not working.
Is it possible that I am configuring it incorrectly, is there a working example on stm32f207ZG?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.