2018-10-14 10:31 PM
i complied the keil code in the following path C:\Users\staff\Downloads\en.i-cube_lrwan\STM32CubeExpansion_LRWAN_V1.2.0\Projects\B-L072Z-LRWAN1\Applications\LoRa\AT_Slave\MDK-ARM\lora.uvprojx file and hex code was created.
C:\Users\staff\Downloads\en.i-cube_lrwan\STM32CubeExpansion_LRWAN_V1.2.0\Projects\B-L072Z-LRWAN1\Applications\LoRa\AT_Slave\MDK-ARM\mlm32l07x01\lora.hex was put into Lora device using flash loader demonstrator.
but the at commands don't work on the devices.
Any help is appreciated.
2018-10-14 10:50 PM
Use the debugger built onto the board, review the USART and baud rate settings. Watch also that the VCP and shield share some connectivity. Review the schematic.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.