2018-09-02 2:07 AM
hello you guies.
i am tring to erase my flash memory of STM32F767 Nucleo-144 board but i couldn't do that.
That's because my STM32F767 Nucleo-144 board could not be operation right. As soon as i set STRT bit of Flash control register (FLASH_CR) but STM32F767 Nucleo-144 board try to reset. (i confirmed that NRST pin is 3.3V --> 0V and than 3.3V.)
if you guies have any great ideas, please let me know.
thank you so much your effort,
My source code is below:
1. single memory bank: 2Mbyte.
2. I am using the HAL_StatusTypeDef HAL_FLASHEx_Erase(FLASH_EraseInitTypeDef *pEraseInit, uint32_t *SectorError)).
3. Memory addresss configure:
// Base address of the Flash sectors
#define ADDR_FLASH_SECTOR_0 ((uint32_t)0x08000000) //Sector 0, 32 Kbytes
#define ADDR_FLASH_SECTOR_1 ((uint32_t)0x08008000) //Sector 1, 32 Kbytes
#define ADDR_FLASH_SECTOR_2 ((uint32_t)0x08010000) //Sector 2, 32 Kbytes
#define ADDR_FLASH_SECTOR_3 ((uint32_t)0x08018000) //Sector 3, 32 Kbytes
#define ADDR_FLASH_SECTOR_4 ((uint32_t)0x08020000) //Sector 4, 128 Kbytes
#define ADDR_FLASH_SECTOR_5 ((uint32_t)0x08040000) //Sector 5, 256 Kbytes
#define ADDR_FLASH_SECTOR_6 ((uint32_t)0x08080000) //Sector 6, 256 Kbytes
#define ADDR_FLASH_SECTOR_7 ((uint32_t)0x080C0000) //Sector 7, 256 Kbytes
#define ADDR_FLASH_SECTOR_8 ((uint32_t)0x08100000) //Sector 8, 256 Kbytes
#define ADDR_FLASH_SECTOR_9 ((uint32_t)0x08140000) //Sector 9, 256 Kbytes
#define ADDR_FLASH_SECTOR_10 ((uint32_t)0x08180000) //Sector 10, 256 Kbytes
#define ADDR_FLASH_SECTOR_11 ((uint32_t)0x081C0000) //Sector 11, 256 Kbytes
#define FLASH_SECTOR_0 ((uint32_t)0U) /*!< Sector Number 0 */
#define FLASH_SECTOR_1 ((uint32_t)1U) /*!< Sector Number 1 */
#define FLASH_SECTOR_2 ((uint32_t)2U) /*!< Sector Number 2 */
#define FLASH_SECTOR_3 ((uint32_t)3U) /*!< Sector Number 3 */
#define FLASH_SECTOR_4 ((uint32_t)4U) /*!< Sector Number 4 */
#define FLASH_SECTOR_5 ((uint32_t)5U) /*!< Sector Number 5 */
#define FLASH_SECTOR_6 ((uint32_t)6U) /*!< Sector Number 6 */
#define FLASH_SECTOR_7 ((uint32_t)7U) /*!< Sector Number 7 */
#define FLASH_SECTOR_8 ((uint32_t)8U) /*!< Sector Number 8 */
#define FLASH_SECTOR_9 ((uint32_t)9U) /*!< Sector Number 9 */
#define FLASH_SECTOR_10 ((uint32_t)10U) /*!< Sector Number 10 */
#define FLASH_SECTOR_11 ((uint32_t)11U) /*!< Sector Number 11 */
uint16_t Flash_Erase_Init(void) {
FLASH_EraseInitTypeDef pErase;
static uint32_t SectorError = 0;
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR
| FLASH_FLAG_PGAERR | FLASH_FLAG_PGPERR | FLASH_FLAG_ERSERR);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_WWDG, DISABLE);
pErase.TypeErase = FLASH_TYPEERASE_SECTORS;
pErase.Sector = FLASH_SECTOR_8;
pErase.NbSectors = FLASH_SECTOR_10;
pErase.VoltageRange = FLASH_VOLTAGE_RANGE_3;
uint16_t res = HAL_FLASHEx_Erase(&pErase,&SectorError);
if (res != HAL_OK) {
return res;
}
RCC_APB1PeriphClockCmd(RCC_APB1Periph_WWDG, ENABLE);
return HAL_OK;
}
2018-09-02 8:58 AM
pErase.NbSectors = FLASH_SECTOR_10; // This looks bogus, try = 1
RCC_APB1PeriphClockCmd(RCC_APB1Periph_WWDG, DISABLE); // Can you turn off the watchdog?
Try building/testing the example
STM32Cube_FW_F7_V1.12.0\Projects\STM32F767ZI-Nucleo\Examples\FLASH\FLASH_EraseProgram\Src\main.c
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.