2012-08-11 12:46 AM
About 45 minutes into playing with my new VLDiscovery board, I seem to have bricked it. I downloaded a ''bad'' program onto the thing and now it's telling me that the device is protected and resists all my attempts to put a ''good'' program into flash.
I'm doing all this on OS X (Lion) with opened 0.6.0-rc1. Openocd seemed to work well enough to put the bad code down, so I've got to believe there's some magic incantation that will let me use the same setup to get it working again. The board cost less than $10, but it'd be a shame to throw it away because of some bad bits. I'm pretty sure my opened setup is workable because I can successfully flash a STMF4Discovery board with good code. What I'm missing is some way to bring the VLDiscovery board back.Unfortunately, I don't have access to a windows environment and CrossWorks chokes when I try to install the STM32 packages and thus never sees my board via USB.The board seems generally hosed now with bogus values coming back for the size of flash memory. Is it just a paperweight now?--------------------------------------$ telnet localhost 4444Trying 127.0.0.1...Connected to localhost.Escape character is '^]'.Open On-Chip Debugger> halttarget was in unknown state when halt was requestedtarget state: haltedtarget halted due to debug-request, current mode: Thread xPSR: 0x01000000 pc: 0xfffffffe msp: 0xfffffffc> mdw 0 4 0x00000000: 40000080 00000000 00000000 00000000 > flash erase_sector 0 0 lastdevice id = 0x10016420flash size = 5384kbyteserased sectors 0 through 5383 on flash bank 0 in 0.029046s> cd /Users/andy/code/chibios/demos/ARMCM3-STM32F100-DISCOVERY> flash write_image build/ch.elfPadding image section 0 with 4 bytesflash write algorithm aborted by targettarget state: haltedtarget halted due to breakpoint, current mode: Thread xPSR: 0x41000000 pc: 0x2000003a msp: 0xfffffffcflash write failed at address 0x8000002flash memory write protectederror writing to flash at address 0x08000000 at offset 0x00000000in procedure 'flash'2012-08-27 6:00 PM
I am looking for the jumper for BOOT0...
In the case of the VL, with some micro gripper probes attached to the BOOT0 pin and the 3V pin.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.