2021-08-09 8:01 AM
#include "stm32l4xx.h"
#include <stdint.h>
#define SYS_FREQ 16000000
#define APB1_CLK SYS_FREQ
#define UART_BaudRate 115200
#define GPIOAEN (1U<<0)
#define UART2EN (1U<<17)
#define CR1_TE (1U<<3)
#define CR1_UE (1U<<0)
#define ISR_TXE (1U<<7)
static void uart_setBaudRate (USART_TypeDef *USARTx, uint32_t PeriphClk, uint32_t BaudRate);
static uint16_t compute_uart_bd(uint32_t PeriphClk, uint32_t BaudRate);
void uart2_tx_init(void);
void uart2_write(int ch);
int main(void){
uart2_tx_init();
while(1){
uart2_write('Y');
}
}
void uart2_tx_init(void)
{
/************Configure GPIO pin**************************/
/*Enable clock access to gpioA*/
RCC->AHB2ENR |=GPIOAEN;
/*Set PA2 mode to alternate function type*/
GPIOA->MODER &=~(1U<<4);
GPIOA->MODER |=(1U<<5);
/*Set PA2 alternate mode to uartTX AFO7*/
GPIOA->AFR[0] |=(1U<<8);
GPIOA->AFR[0] |=(1U<<9);
GPIOA->AFR[0] |=(1U<<10);
GPIOA->AFR[0] &=~(1U<<11);
/************Configure UART mode**************************/
/*Enable Clock acess ti uart2*/
RCC->APB1ENR1 |=UART2EN;
/*Configure Baudrate*/
uart_setBaudRate(USART2,APB1_CLK,UART_BaudRate);
/*Configure the transfer direction*/
USART2->CR1 = CR1_TE;
/*Enable usart module*/
USART2->CR1 |= CR1_UE;
}
void uart2_write(int ch){
/*Make sure transmit data register is empty*/
while(!(USART2->ISR & ISR_TXE)){}
/*Write to transmit data register*/
USART2->TDR = (ch & 0xFF);
}
static void uart_setBaudRate (USART_TypeDef *USARTx, uint32_t PeriphClk, uint32_t BaudRate){
USARTx->BRR = compute_uart_bd(PeriphClk,BaudRate);
}
static uint16_t compute_uart_bd(uint32_t PeriphClk, uint32_t BaudRate)
{
return ((PeriphClk +(BaudRate/2U))/BaudRate);
}
2021-08-09 8:34 AM
a) Use STM32CubeMX to generate initialization code for your STM32 pinout, and check if you missed anything.
b) Look at the tutorials for sample UART code.
c) Attached project in C++ using STM32CubeMX has some useful startup code: STM32L476RG-Nucleo_TestsPR06.zip
*I suggest C++ for the enhanced compile time checking, even if everything is just C Code.
d) Did you make your own PCB or are you using a standard board like a Nucleo? What is the STM32 pinout and schematic?
*When posting code use the </> in toolbar so code keeps formatting and is easier to read.
Paul
2022-04-09 12:43 AM
@Charlie4918 : Can you please tell me why the equation return ((PeriphClk +(BaudRate/2U))/BaudRate); was used?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.