2020-03-25 10:43 AM
Here is my system clock config, my Timer 2 initialization, and the read function.
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;
__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 216;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 9;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
HAL_PWREx_ActivateOverDrive();
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV8;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV4;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7);
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART3|RCC_PERIPHCLK_CLK48;
PeriphClkInitStruct.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1;
PeriphClkInitStruct.Clk48ClockSelection = RCC_CLK48SOURCE_PLL;
HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct);
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_TIM;
PeriphClkInitStruct.TIMPresSelection = RCC_PERIPHCLK_TIM;
// PeriphClkInit.TIMPresSelection = RCC_USART2CLKSOURCE_PCLK1;
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 15, 0);
}
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
uint8_t error_count;
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 0;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 0;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.RepetitionCounter = 20;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
error_count++;
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
error_count++;
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
error_count++;
}
/* USER CODE BEGIN TIM2_Init 2 */
/* USER CODE END TIM2_Init 2 */
}
uint16_t read_TIM2() {
return TIM2->CNT;
}
2020-03-25 10:59 AM
>>htim2.Init.Period = 0;
Surely this is going to be constraining?
Not sure what part you're using, but lets guess this is a 32-bit timer
htim2.Init.Period = 0xFFFFFFFF;
If all the TIM2 registers are zero, check you've enabled the APB clock for TIM2 properly. Review peripheral register in a debugger.
2020-03-25 1:18 PM
Its a 16 bit timer right now.
I tried
htim2.Init.Period = 0xFFFF;
I also used the
__HAL_RCC_TIM2_CLK_ENABLE();
I verified that the APB1ENR bit 0 is set to 1
Unfortunately the timer is not running.
TMR2->CNT = 0
2020-04-15 7:56 AM
I think you are missing the HAL_TIM_Base_Start(&htim2) call. You just initialized the counter, but did not start it.
But I have the same problem even with the timer being started. Did you get your timer to work? If yes i would like to know what you changed :)
2020-04-15 3:53 PM
Read out and check/post the TIM registers' content.
If they are all 0, check in RCC if its clock has been enabled (again, by reading out and checking the respective RCC_APBxENR).
JW
2020-04-16 5:22 AM
I found the mistake, i had configured the timer wrong (SlaveMode). (But the mistake is not existent in the code of CMysz.1, i guess he just forgot the HAL_TIM_Base_Start() call).
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.