2023-01-12 2:40 PM
I am using a U585QI and have some external flash memory connected to an OCTOSPI. We are having some intermittent failures with it, and since we're powering the processor with 1.8v I want to try enabling HSLV for the Data/Clock lines. I found HAL_GPIO_EnableHighSPeedLowVoltage, but I'm not sure when to call it...
1) Is this a common use case for the high-speed-low-voltage functionality?
2) Is there any example code for this? Particularly the option bits aspect?
Solved! Go to Solution.
2023-01-18 5:41 AM
Hello,
This is an example of OCTOSPI with HSLV configuration
/**
* @brief OSPI MSP Initialization
* This function configures the hardware resources used in this example
* @param hospi: OSPI handle pointer
* @retval None
*/
void HAL_OSPI_MspInit(OSPI_HandleTypeDef* hospi)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(hospi->Instance==OCTOSPI1)
{
/* USER CODE BEGIN OCTOSPI1_MspInit 0 */
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_CS_GPIO_PORT, OCTOSPI_CS_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_DQS0_GPIO_PORT, OCTOSPI_DQS0_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_DQS1_GPIO_PORT, OCTOSPI_DQS1_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_CLK_GPIO_PORT, OCTOSPI_CLK_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_NCLK_GPIO_PORT, OCTOSPI_NCLK_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D0_GPIO_PORT, OCTOSPI_D0_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D1_GPIO_PORT, OCTOSPI_D1_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D2_GPIO_PORT, OCTOSPI_D2_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D3_GPIO_PORT, OCTOSPI_D3_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D4_GPIO_PORT, OCTOSPI_D4_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D5_GPIO_PORT, OCTOSPI_D5_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D6_GPIO_PORT, OCTOSPI_D6_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D7_GPIO_PORT, OCTOSPI_D7_PIN);
/* USER CODE END OCTOSPI1_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_OSPI;
PeriphClkInit.OspiClockSelection = RCC_OSPICLKSOURCE_SYSCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_OSPIM_CLK_ENABLE();
__HAL_RCC_OSPI1_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/**OCTOSPI1 GPIO Configuration
PC0 ------> OCTOSPIM_P1_IO7
PC1 ------> OCTOSPIM_P1_IO4
PC2 ------> OCTOSPIM_P1_IO5
PA7 ------> OCTOSPIM_P1_IO2
PC3 ------> OCTOSPIM_P1_IO6
PB0 ------> OCTOSPIM_P1_IO1
PB2 ------> OCTOSPIM_P1_DQS
PA2 ------> OCTOSPIM_P1_NCS
PA3 ------> OCTOSPIM_P1_CLK
PA6 ------> OCTOSPIM_P1_IO3
PB1 ------> OCTOSPIM_P1_IO0
*/
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF3_OCTOSPI1;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_2|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* USER CODE BEGIN OCTOSPI1_MspInit 1 */
/* USER CODE END OCTOSPI1_MspInit 1 */
}
}The High speed low voltage (HSLV) is a feature, when enabled it allow the GPIOs to reach higher frequencies. The only constraint is that Vdd must not exceed 2.5v (Vdd < 2.5v)
Mohamed Aymen
2023-01-16 8:14 AM
Hello @Community member and welcome to the community,
You need to enable HSLV of OCTOSPI pins before initializing its pins.
Mohamed Aymen
2023-01-16 9:17 AM
@Mohamed Aymen HZAMI Does that mean calling HAL_GPIO_EnableHighSPeedLowVoltage before HAL_OSPI_Init? And does it mean I need to do it to run OSPI from a 1.8v VDD reliably?
2023-01-18 5:41 AM
Hello,
This is an example of OCTOSPI with HSLV configuration
/**
* @brief OSPI MSP Initialization
* This function configures the hardware resources used in this example
* @param hospi: OSPI handle pointer
* @retval None
*/
void HAL_OSPI_MspInit(OSPI_HandleTypeDef* hospi)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(hospi->Instance==OCTOSPI1)
{
/* USER CODE BEGIN OCTOSPI1_MspInit 0 */
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_CS_GPIO_PORT, OCTOSPI_CS_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_DQS0_GPIO_PORT, OCTOSPI_DQS0_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_DQS1_GPIO_PORT, OCTOSPI_DQS1_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_CLK_GPIO_PORT, OCTOSPI_CLK_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_NCLK_GPIO_PORT, OCTOSPI_NCLK_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D0_GPIO_PORT, OCTOSPI_D0_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D1_GPIO_PORT, OCTOSPI_D1_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D2_GPIO_PORT, OCTOSPI_D2_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D3_GPIO_PORT, OCTOSPI_D3_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D4_GPIO_PORT, OCTOSPI_D4_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D5_GPIO_PORT, OCTOSPI_D5_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D6_GPIO_PORT, OCTOSPI_D6_PIN);
HAL_GPIO_EnableHighSPeedLowVoltage(OCTOSPI_D7_GPIO_PORT, OCTOSPI_D7_PIN);
/* USER CODE END OCTOSPI1_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_OSPI;
PeriphClkInit.OspiClockSelection = RCC_OSPICLKSOURCE_SYSCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_OSPIM_CLK_ENABLE();
__HAL_RCC_OSPI1_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/**OCTOSPI1 GPIO Configuration
PC0 ------> OCTOSPIM_P1_IO7
PC1 ------> OCTOSPIM_P1_IO4
PC2 ------> OCTOSPIM_P1_IO5
PA7 ------> OCTOSPIM_P1_IO2
PC3 ------> OCTOSPIM_P1_IO6
PB0 ------> OCTOSPIM_P1_IO1
PB2 ------> OCTOSPIM_P1_DQS
PA2 ------> OCTOSPIM_P1_NCS
PA3 ------> OCTOSPIM_P1_CLK
PA6 ------> OCTOSPIM_P1_IO3
PB1 ------> OCTOSPIM_P1_IO0
*/
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF3_OCTOSPI1;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_2|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* USER CODE BEGIN OCTOSPI1_MspInit 1 */
/* USER CODE END OCTOSPI1_MspInit 1 */
}
}The High speed low voltage (HSLV) is a feature, when enabled it allow the GPIOs to reach higher frequencies. The only constraint is that Vdd must not exceed 2.5v (Vdd < 2.5v)
Mohamed Aymen
2023-01-18 6:12 AM
Awesome, thank you! Can you confirm that this is something I should be doing to get reliable OSPI communication when powered at 1.8v?
2023-01-30 1:55 AM
Hello @Community member,
If you are targeting higher frequencies at Vdd < 2.5V, yes it is recommended to Enable the HSLV.
Mohamed Aymen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.