2020-11-16 5:26 AM
HSI or HSE ?
carefully read the pictures
2020-11-16 7:08 AM
The HSI/2 divider is fixed. See PLLSRC description.
PLLXTPRE is a copy of 0th bit of PREDIV (for historical reasons) - it's quite clearly written in description of both fields.
JW
2020-11-16 7:11 AM
in the picture, HSE is divided once, but the text shows that the second divisor by 2 is hidden somewhere, but it is not in the scheme. but there is an HSI divider that, judging by the bits, can be configured.
2020-11-16 7:28 AM
No, the register here reflects two copies of the same bit.
The HSI is divided by TWO, always,as it comes from a pulse generator, and doesn't have the prerequisite 50/50 duty.
For the purpose of setting the PLL assume the HSI/2 input is always 4 MHz
2020-11-16 7:37 AM
thanks
here is a piece of text that I overlooked:
This bit is the same as the LSB of PREDIV in Clock configuration register 2
(RCC_CFGR2) (for compatibility with other STM32 products)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.