2021-03-08 6:22 AM
Hello,
I have faced quite interesting problem when i try to obtain the pwm out on the Nucleo board. I use CubeMx to config and I set the HRTimer clock as cpu_clock (480 MHz) . When I run the code, I only get the half clock frequency driven pwm out (240 MHz) even I had no prescaler (no division selection) . I assume that the resulting maximum clock frequency of HRTimer is 240 MHz.
What should be wrong with my application, what am I missing ?
Thanks and regards,
DH..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.