2015-02-17 6:54 AM
Hi all! I'm a bit confused by USB Host behaviour when trying to enable Suspend mode.
I use ST USB library v.2.1.0. and STM32F407. Use Host example for HID device, and it is working correct. Now I try to make some changes - suspend and resume connected device.I just write suspend enable bit in Host Port control and status register: *pdev->regs.HPRT0 |= (1 << 7);I see by the oscilloscope, that host really stops sending SOFs after that action, bus seems to be in idle state. At the same time I see at the value of HPRT0 register, that Suspend bit was not asserted to 1. Instead of it I see ''Port enable'' bit falls to 0, and according Port interrupt cames. In the result, write to Resume bit have no effect: no life on DP-DM accures after that. So, I can enable port just by Reset - that is, by restarting device. But I needed just Suspend-Resume.It also seems strange, that in library there are no functions for Suspending-Resuming the device. Maybe, this functions are not really supported? Or I forget do some additional settings?I would be extremely thankful, if someone shares working code examples for enabling and disabling Suspend mode by the USB Host Controller in STM32F4-devices. Or gives any advice on this topic.2015-05-10 7:33 PM
Hi alexey,
Did you clear this problem already? I faced same problem last week and I cleared this. I think that this problem is Specification documentation error. PENA is rc_w1, rc_w0 is wrong. Please try PSUSP(HPRT bit7)=1 with PENA(HRRT bit2)=0. Regards2015-07-21 1:43 AM
Hi! Thanks for reply. It is correct solution - I've also found this feature of PENA bit eventually.
Seems to be not very convenient to write to HPRT - we must always remember about not writing 1 to PENA, if we don't want Port to be disabled.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.