2017-03-10 12:54 AM
Hello, How do I write a variable to the SRAM2 on an STM32L476 ? I am putting the uC in the Standby mode and I am preserving the SRAM2 memory, but I cannot manage to write to it. I am trying like this:
&sharpdefine VAR_LOC ((volatile uint8_t *)(0x10000000))
volatile uint8_t *pVar = VAR_LOC;(*pVar)++;
Do I need to active some clock for the SRAM2 memory?
Thanks! Any information is helpful.
#stm32l4 #sram2 #standbymode2017-03-10 1:25 AM
In your project file there is a linker file which describe the various memory sections.
Find which name is for SRAM2 and then dig in the #pragma of your compiler to tell at compile time that the following variables are to be put in the corresponding section.
This is toolchain dependent.
If there is a Cube example, then it should be easy.
Here for illustrative purpose, an IAR linker configuration file: (icf file)
/*###ICF### Section handled by ICF editor, don't touch! ****/
/*-Editor annotation file-*//* IcfEditorFile='$TOOLKIT_DIR$\config\ide\IcfEditor\cortex_v1_0.xml' *//*-Specials-*/define symbol __ICFEDIT_intvec_start__ = 0x08000000;/*-Memory Regions-*/define symbol __ICFEDIT_region_ROM_start__ = 0x08000000;define symbol __ICFEDIT_region_ROM_end__ = 0x080FFFFF;define symbol __ICFEDIT_region_RAM_start__ = 0x20000000;define symbol __ICFEDIT_region_RAM_end__ = 0x2001FFFF;define symbol __ICFEDIT_region_CCMRAM_start__ = 0x10000000;define symbol __ICFEDIT_region_CCMRAM_end__ = 0x1000FFFF;/*-Sizes-*/define symbol __ICFEDIT_size_cstack__ = 0x800;define symbol __ICFEDIT_size_heap__ = 0x400;/**** End of ICF editor section. ###ICF###*/define memory mem with size = 4G;define region ROM_region = mem:[from __ICFEDIT_region_ROM_start__ to __ICFEDIT_region_ROM_end__];define region RAM_region = mem:[from __ICFEDIT_region_RAM_start__ to __ICFEDIT_region_RAM_end__];define region CCMRAM_region = mem:[from __ICFEDIT_region_CCMRAM_start__ to __ICFEDIT_region_CCMRAM_end__];define block CSTACK with alignment = 8, size = __ICFEDIT_size_cstack__ { };
define block HEAP with alignment = 8, size = __ICFEDIT_size_heap__ { };initialize by copy { readwrite };
do not initialize { section .noinit };place at address mem:__ICFEDIT_intvec_start__ { readonly section .intvec };
place in ROM_region { readonly };
place in RAM_region { readwrite, block CSTACK, block HEAP };2017-03-10 1:32 AM
2017-03-16 8:16 AM
Thanks for all the answers!
I will answer my own question:
No, you do not need to manually start any clock for the SRAM. I was just reading back the variable in the wrong way.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.