2020-12-09 11:38 AM
2020-12-09 11:41 AM
I realize this isn't STM32 specific, but that's what I am using. I would like to learn from examples where ports and data are changeable at run-time. I know I need to use a pointer, but I'm not sure how to proceed. So a chunk of code at one boot might write data out UART1, then after user config and next boot, UART2 or both or whatever.
Edit: Preferably there would only be one set of UART functions for initialization, read, write, etc. These would use the appropriate data and hardware depending on the configuration.
2020-12-09 2:46 PM
The things are instances/objects to start with. The normal approach is to pass around a pointer rather than use a global.
UART_HandleTypeDef Uart[1] = {0};
void InitUart(UART_HandleTypeDef *UartInstance, USART_TypeDef *Uart, uint32_t BaudRate)
{
UartInstance->Instance = Uart;
UartInstance->Init.BaudRate = BaudRate;
UartInstance->Init.WordLength = UART_WORDLENGTH_8B;
UartInstance->Init.StopBits = UART_STOPBITS_1;
UartInstance->Init.Parity = UART_PARITY_NONE;
UartInstance->Init.HwFlowCtl = UART_HWCONTROL_NONE;
UartInstance->Init.Mode = UART_MODE_TX_RX;
UartInstance->Init.OverSampling = UART_OVERSAMPLING_16;
#ifdef UART_ONE_BIT_SAMPLE_DISABLE
UartInstance->Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
#endif
if (HAL_UART_Init(UartInstance) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
}
void OutString(UART_HandleTypeDef *UartInstance , char *s)
{
HAL_UART_Transmit(UartInstance, (uint8_t *)s, strlen(s), 5000);
}
InitUart(Uart, USART2, 115200);
OutString(Uart,"Hello World!\n");
2020-12-10 6:43 AM
Thanks, Yes, this is what I was concerned about. If a process has data it can't just enqueue it Enqueue(theData), it has to pass around the instance as you say, Enqueue(theInterface, theData), so it still needs to specify which Uart. Hmmm. I also have some interfaces that are bit-bang port things, so I want to make it as clean as possible for the higher layers. Like for example, a byte might be going out a UART or USB CDC VCOM or even something else. I don't want to have to have to use switch statements all over the place where it decides at run-time which interface to receive the data.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.