2015-09-19 5:30 AM
I need to call several CDC_Transmit_FS, but between them I need to wait to previous CDC_Transmit_FS finish, otherwise I overwrite output buffer.
Is there a flag, a macro or something else that may allows me to determine CDC_Transmit_FS in progress or finish?Thank!2015-10-02 4:26 AM
Hi elgarbe,
You can manage several CDC_Transmit calls based on the USBH_CDC_TransmitCallback.In this callback function, you can call the CDC_Transmit functions as it is done in the example STM32Cube_FW_F4_V1.8.0\Projects\STM324xG_EVAL\Applications\USB_Host\CDC_Standalone (have a look to the implementation in Src/cdc_send.c).-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-10-02 5:47 AM
is it work on Device mode too?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.