2019-08-22 4:13 AM
Hello,
I've configured the stm32h743 to write on a paticular adress without incrementing it and was also successful in it.
The problem is no matter how many times i call HAL_SRAM_Read_DMA(...) it will not start a new transfer.
In the trainings Manual they say that "the channel will be disabled after the transfer", although i need it to continue transfering Data.
have someone experienced the same behavior?
2019-09-16 12:48 AM
After Struggling to get the answer i finally found the problem.
The MDMA was not linked to a Parent process.
Use: __HAL_LINKDMA(__HANDLE__, __PPP_DMA_FIELD__, __DMA_HANDLE__) to solve this.
thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.