2019-05-17 5:56 AM
When I cut the STLINK module the nucléo board don't work
It whork's before cut
External power E5V
Thank you
2019-05-17 6:11 AM
Double check that when cutting you did not harm other parts.
2019-05-17 7:39 AM
What kind of diagnostic output does you code provide to know if it is actually running or not?
If you reconnect the ST-LINK via the SWD header and pins on the target side, can you connect then?
2019-05-17 10:46 AM
There is no external clock source on the Nucleo 767 when you disconnect the ST-LINK. To make it work you must code to use the internal RC oscillator. I've done this and it works fine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.