2019-08-07 7:48 AM
There are 3 interrupt handler EXTI0__1 ,EXTI2__3, EXTI 14__5
how they can be used since it can be working in EV board but i am not able to work it in STM32F3K6
2019-08-07 8:22 AM
Just modify some of the existing examples.
EXTI0__1 sinks EXTI0 and EXTI1 interrupt sources
EXTI 14__5 sinks EXTI5, EXTI6, EXTI7, EXTI8, EXTI9, EXTI10, EXTI1, EXTI2, EXTI3, and EXTI4, ie from GPIO_PINS 5..14 (ONE PIN/BANK per source)
2019-08-07 10:29 PM
Sir,
If I want to take PA3 pin as external interrupt and take decision on PA9 pin than which EXTI__ will be use and how i can select them.
Please help me in understanding this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.