2009-12-06 3:07 AM
How to trigger the EXTI_Line18 event/USBWakeup IRQ
2011-05-17 4:32 AM
I'm trying to put my application into STOP mode and then use the EXTI_Line18 to trigger the USBWakeup IRQ.
Does anyone know what events will cause the EXTI_Line18 to create an interrupt that will then trigger USBWakeup? I've seen mention that the USB cable being attached will do this, but because I am developing a bus-powered device this would be the same for me as a power off/power on. Are there are any other events I can use? My USB device is HID based and I have a test tool that I can use to send/receive commands at the application level. However, once I enter STOP mode the USB device disappears from my Windows Device Manager (because the USB ISR is not being serviced?) Any thoughts welcome, SteveO.2011-05-17 4:32 AM
The USB suspend/resume is described in USB specification and it is used if ie. PC goes to stand-by.
Then PC host stops giving periodic packets, after 3 ms all devices must enter low-power mode (avg. < 0.5 mA). When PC wakes up, it restarts the USB comm. and the devices restart with resume event.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.