2021-11-19 1:13 AM
Hi, i try to using QSPI in STM32H743( the STM32H743_Nucleo ) to received data, the programming IDE is STM32CubeIDE, and i used it to generated and assign pin and parameter. The clock and NCS pin is probed to oscilloscope, the code is as followed, when the program started, i can not see the clock and NCS shown in the oscilloscope, the NCS is always high and no clock signal, do i miss something to setup or coding ?
Best Regards
thank you
int main(void)
{
/* USER CODE BEGIN 1 */
int i;
/* USER CODE END 1 */
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
//MX_USART3_UART_Init();
MX_QUADSPI_Init();
MX_I2C1_Init();
MX_I2C2_Init();
/* USER CODE BEGIN 2 */
hqspi_cmdX.Instruction=0x80;
hqspi_cmdX.InstructionMode=QSPI_INSTRUCTION_1_LINE;
hqspi_cmdX.Address=0x000000;
hqspi_cmdX.AddressSize =QSPI_ADDRESS_24_BITS;
hqspi_cmdX.AddressMode=QSPI_ADDRESS_1_LINE;
hqspi_cmdX.AlternateByteMode=QSPI_ALTERNATE_BYTES_NONE;
hqspi_cmdX.DummyCycles=0x00;
hqspi_cmdX.DataMode=QSPI_DATA_4_LINES;
hqspi_cmdX.DdrMode=QSPI_DDR_MODE_DISABLE;
hqspi_cmdX.NbData=9600*4;//number of data to Xfer
hqspi_cmdX.SIOOMode=QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &hqspi_cmdX, 100 )!=HAL_OK){
Error_Handler();
}
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
HAL_Delay(500);
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET);
HAL_Delay(500);
do {
HAL_Delay(5);
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET);
HAL_Delay(3);
HAL_QSPI_Receive(&hqspi, buffer, 5);//?
HAL_Delay(10);
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
HAL_Delay(10);
}while(1);
}
/* USER CODE END 3 */
}
static void MX_QUADSPI_Init(void)
{
/* USER CODE BEGIN QUADSPI_Init 0 */
__HAL_RCC_QSPI_FORCE_RESET();
__HAL_RCC_QSPI_RELEASE_RESET();
/* USER CODE END QUADSPI_Init 0 */
/* USER CODE BEGIN QUADSPI_Init 1 */
/* USER CODE END QUADSPI_Init 1 */
/* QUADSPI parameter configuration*/
hqspi.Instance = QUADSPI;
hqspi.Init.ClockPrescaler = 12;
hqspi.Init.FifoThreshold = 1;
hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_HALFCYCLE;
hqspi.Init.FlashSize = 12;
hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_5_CYCLE;
hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
hqspi.Init.DualFlash = QSPI_DUALFLASH_ENABLE;
if (HAL_QSPI_Init(&hqspi) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN QUADSPI_Init 2 */
/* USER CODE END QUADSPI_Init 2 */
}
2021-12-08 6:36 AM
Hello @cchan.2,
The Nucleo-H743ZI board does not embed Quad-SPI Flash memory, so it is necessary to connect an external memory following the hardware configuration needed.
Chahinez.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.