2025-05-30 4:12 AM
Core : STM32H743Z , STM32H753V, STM32H750 @ 480MHz
External Sync Clock (as EXTI0): 10Mhz
I tried to read/write GPIO ports with TIM2_UP and TIM3_UP events, in sync with an external clock. Data transfer (both in and out) is taking place, but not synchronised with EXTI.
EXTIx 'events' are not triggering. Howvere EXTI 'interrupt' is working but the maximum data rate is less than 3MHZ
Basic code initiated by CubeMX.
Is there any working example for GPIO read with DMA and EXTI ?
Thanks for your help in advance!
2025-05-30 5:56 AM
So it's working but not as fast as you would like? That's due to the system architecture. The GPIO is separated from the CPU by a bus. There are other chips that would be better for this. Consider instead using an interface like QSPI or FMC if possible.
2025-05-31 4:20 AM - edited 2025-05-31 4:28 AM
I am getting 150% of the required transfer speed without any missing codes. Verified with 0 to 65535 in Circualr DMA mode, (asynchronous with master). But the issue is in the syncronisation of salve with master. First few half wrods are missing (only) in start of transmisssion.
2025-06-01 3:39 AM
> I tried to read/write GPIO ports with TIM2_UP and TIM3_UP events, in sync with an external clock.
Then maybe set the external clock as source for the timer?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.