2012-09-26 5:37 AM
Hello all,
I am doing a project where the microcontroller (STM32) is sending the parameters to the server via DHCP using wifi module. So, now i want to make available an offline web page to the user where he will put the SSID and phrase of the DHCP. This web page will be stored in the microcontroller and when the user connects the device to the PC using USB, folder containing this webpage should appear on the screen. Can anybody help me out on how do i do this? Thank you. #learn-to-walk-before-running #dhcp #drowning #drowning #http #html2012-09-29 3:45 AM
''the microcontroller (STM32) is sending the parameters to (sic?) the server via DHCP''
Don't you have that back-to-front? Surely, a DHCP server supplies parameters to the client (in this case, the STM32) ??
http://en.wikipedia.org/wiki/Dynamic_Host_Configuration_Protocol
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.