2020-10-21 9:04 PM
I am using STM32L442KC part number...And i want to store the 16 byte of data on non erasable memory of controller during runtime...Can i get any reference how to store the data in microcontroller memory???
2020-10-21 9:15 PM
Which OPT bytes would these be?
2020-10-22 6:02 AM
You can use the EEProm emulation software, or you can roll your own solution:
You need to erase the flash page and program your data each time you want to change it.
2020-10-24 12:42 AM
Hi TDK,
Thanks for your reply...
I have downloaded the EEProm emulation software(X-CUBE-EEPROM_V2.0.0). But in that there are so many files found in project folder of my targeted microcontroller.
I am stuck up with how to use that files in my actual code....
if any reference for how to use this files will be very helpful for me....
2020-10-27 3:12 AM
I am targeted for the STM32L442KC part number... But in "X-CUBE-EEPROM_V2.0.0\Projects\STM32L4\EEPROM_Emul" folder I found the readme in which mentioned that "This example runs on STM32L476xx devices and STM32L4R5xx devices." will it work for STM32L442KC???
Also i didn't found eeprom.c file to use the respective API related to EEPROM....
2020-10-27 3:47 AM
The exact option byte/address has not been decided yet...the actual requirement is during runtime client system is going to send one string to my system and i have to store that string at non erasable memory to use afterward for further processing....I am stuck with how to store that received data in internal non erasable memory...
I found some API during search EEPROM_WriteData(), EEPROM_ReadData().... but stuck at how to generate the related API or middleware..
2020-10-27 6:43 AM
I don't use the EEPROM emulation software myself. I do have the same thing working on a few projects, but with my own code. I would imagine the code works on a STM32L442KC with few changes, but I'm guessing here.
2020-10-28 1:33 AM
Have you written on internal EEPROM in your code??if yes, how you have did this?? So that i can try the same logic in my code.
I am using STM32L442KC with AES functionality used in it...
2020-10-28 7:09 AM
2020-11-07 9:06 PM
Hi...
I have tried with below lines.
HAL_FLASH_Unlock();
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, 0x8000001, 0x01);
HAL_FLASH_Lock();
i.e i am trying to write the 0x01 data on address 0x8000001..
Any API to check???whether I have written the correct data on that particular address or not....
or can I read that data using particular API..? so that i can read and print it on Hyper Terminal to cross verify the successful data written on location or not.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.