2019-11-19 8:51 PM
When I connect a voltage source to channel 0 of SDADC2 in single ended mode, then at floating pin and connecting to ground the value displayed is full scale which 65535, while when I connect some voltage like 2V or 3V to same channel then it shows the result fixed as 32738. I checked the software configuration refereing to the Reference Manual and have connected VREF to 3.3V which is VDD.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.