2015-07-03 9:40 AM
Hi
I have succedded in transmitting a SPI message via DMA.It sends the complete array whose length is specified by BufferSize (typically 100 in the examples). This value is assigned, e.g. to DMA BufferSize as DMA_InitStructure.DMA_BufferSize = BUFFER_SPI_SIZE ;Someone know how to specify a different size during run-time by modifying the transmitter configuration (or another solution)? I have tried SPIx_TX_DMA_STREAM->NDTR = new_message_size;SPIx_RX_DMA_STREAM->NDTR = new_message_size;which is equivalent to DMA_InitStructure.DMA_BufferSize = BUFFER_SPI_SIZE ;DMA_Init(SPIx_RX_DMA_STREAM, &DMA_InitStructure);DMA_Init(SPIx_TX_DMA_STREAM, &DMA_InitStructure);in the transmitter (the receiver doesn�t know the length), but it doesn't seem to work.I have read another post in which it is solved via NSS, but I would prefer not to using it.Thanks in advance #spi-dma-stm32-lengthWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.