2016-03-04 11:50 AM
The Cube is not clear in this. I want to output squarewave 1kHz-0.1Hz from a pin. There are no examples about this and explanations are not clear either.
I want to use STM32F1 CPU. #je-ne-l'aime-cube2016-03-04 12:31 PM
PWM with 50/50 duty,Toggle?
2016-03-04 1:19 PM
50% off, 50% on, it is not very critical. What is toggle in this context? Keying or gating with an other signal? Let's keep it simple, I can fine tune details myself, I hope.
2016-03-04 3:56 PM
I found a DM00154093 pdf which talks about the Cube in a way. There is something about timer modes and the Cube tool itself has something similar. I understand a little more about the Cube. I'll try again with the project.
And with extra parenthesis. Code from the Cube: else if((htim->State == HAL_TIM_STATE_READY))2016-03-06 10:50 AM
I found an example which does what I want
STM32Cube_FW_F4_V1.11.0\Projects\STM32F4-Discovery\Examples\TIM\TIM_TimeBase There are no CubeMX projects in those packages. I wonder why. I'll ask ST to include CubeMX projects in their examples.2016-03-07 3:32 AM
Hi mich.lei,
You find the examples for STM32F1 athttp://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF260820
at this path stm32cubef1\STM32Cube_FW_F1_V1.3.0\Projects\STM3210C_EVAL\Examples\TIM
> There are no CubeMX projects in those packages. I wonder why. I'll ask ST to include CubeMX projects in their examples.
The CubeMx does not aim to create a hole project but , infact, it helpsto generate an initialization code to be a start point for the project developement. -Hannibal-2016-03-10 2:43 PM
I just noticed a new post.
We are talking about projects and CubeMx projects. In my opinion Cubemx is a good idea, I mean the visual setup the HW. But it must be used and supported. Giving just initializing code without CubeMx is not so useful, there already is one such interface, I think. Timers have quite many operating modes, so they are one place where CubeMX could help. Besides, Cubemx shows which pins are available and which are taken.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.